SplitSubopCommandLinePlaneTypes Enumeration¶
NXOpen.CAM.SplitSubopCommand.LinePlaneTypes is an alias for NXOpen.CAM.SplitSubopCommandLinePlaneTypes
-
class
NXOpen.CAM.
SplitSubopCommandLinePlaneTypes
¶ Bases:
object
Available line plane types
Enum Members
Enum Member Enum Member Description ParallelToToolaxis Line plane parallel to tool axisNormalToToolaxis Line plane normal to tool axisSpecifyAngle Line plane specify angle-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-