SoftTool Class

class NXOpen.CAM.SoftTool

Bases: NXOpen.CAM.ToolBuilder

Represents a SoftTool

This is an abstract class, and cannot be instantiated.

New in version NX9.0.0.

Properties

Property Description
ChannelName Returns or sets the channel’s name
CutterExportBuilder Returns the cutter export builder
CycleEvent Returns the cycle event
CycleTable Returns the cycle
Description Returns or sets the description
EndUdeSet Returns the end ude set
HolderDescription Returns or sets the holder description
HolderLibraryReference Returns or sets the holder libref
HolderSection Returns the holder sections
LibraryParametersBuilder Returns the Library Data Object
OptimizationMethod Returns or sets the optim method
StartUdeSet Returns the start ude set
Tag Returns the Tag for this object.
TlCtlgNum Returns or sets the Catalog Number
TlDescription Returns or sets the Cutter Description
TlHolderNumberBuilder Returns the Holder Number
TlLibref Returns or sets the Cutter Libref
TlManualToolChange Returns or sets the Manual Tool Change
TlNumberBuilder Returns the Tool Number
TlText Returns or sets the tool text

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetMaterial Get tool material @return
GetMaterialData Get material data
GetObject Returns the object currently being edited by this builder.
SetMaterial Set tool material
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

HolderSection

SoftTool.HolderSection

Returns the holder sections

-------------------------------------

Getter Method

Signature HolderSection()

Returns:
Return type:NXOpen.CAM.HolderSectionBuilder

New in version NX9.0.0.

License requirements: None.

Method Detail

Validate

SoftTool.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.