RotaryPolarMoveBuilder Class¶
-
class
NXOpen.CAM.
RotaryPolarMoveBuilder
¶ Bases:
NXOpen.CAM.MoveBuilder
Represents the Rotary Polar Builder
To create a new instance of this class, use
NXOpen.CAM.MoveCollection.CreateRotaryPolarMoveBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
FeedRate | Returns or sets the feed rate |
FeedType | Returns or sets the feed type |
FeedUnit | Returns or sets the feed unit |
LockAxis | Returns or sets the lock axis |
LockPlane | Returns or sets the lock plane |
LockPos | Returns or sets the lock position |
MotionType | Returns or sets the motion type |
NumberOfUserParameters | Returns the number of user parameters |
OffsetData | Returns the offset point builder |
Point | Returns or sets the location |
ProtectedMove | Returns or sets the protected move status |
RoundPoint | Returns the round point builder |
SubopLabel | Returns or sets the subop label |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetUserParameter | Returns the custom parameter with the given name. |
SetParent | Set parent |
SetSibling | Set sibling |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
RotaryPolarMoveBuilderLockAxisDirection Enumeration | the lock axis type |
RotaryPolarMoveBuilderLockPlaneType Enumeration | the lock plane type |
Property Detail¶
LockAxis¶
-
RotaryPolarMoveBuilder.
LockAxis
¶ Returns or sets the lock axis
-------------------------------------
Getter Method
Signature
LockAxis()
Returns: Return type: NXOpen.CAM.RotaryPolarMoveBuilderLockAxisDirection
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LockAxis(lockAxis)
Parameters: lockAxis ( NXOpen.CAM.RotaryPolarMoveBuilderLockAxisDirection
) –New in version NX5.0.0.
License requirements: None.
LockPlane¶
-
RotaryPolarMoveBuilder.
LockPlane
¶ Returns or sets the lock plane
-------------------------------------
Getter Method
Signature
LockPlane()
Returns: Return type: NXOpen.CAM.RotaryPolarMoveBuilderLockPlaneType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LockPlane(lockPlane)
Parameters: lockPlane ( NXOpen.CAM.RotaryPolarMoveBuilderLockPlaneType
) –New in version NX5.0.0.
License requirements: None.
LockPos¶
-
RotaryPolarMoveBuilder.
LockPos
¶ Returns or sets the lock position
-------------------------------------
Getter Method
Signature
LockPos()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LockPos(lockPosition)
Parameters: lockPosition (float) – New in version NX5.0.0.
License requirements: None.
OffsetData¶
-
RotaryPolarMoveBuilder.
OffsetData
¶ Returns the offset point builder
-------------------------------------
Getter Method
Signature
OffsetData()
Returns: Return type: NXOpen.CAM.OffsetDataBuilder
New in version NX5.0.0.
License requirements: None.
Point¶
-
RotaryPolarMoveBuilder.
Point
¶ Returns or sets the location
-------------------------------------
Getter Method
Signature
Point()
Returns: Return type: NXOpen.Point
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Point(location)
Parameters: location ( NXOpen.Point
) –New in version NX5.0.0.
License requirements: None.
RoundPoint¶
-
RotaryPolarMoveBuilder.
RoundPoint
¶ Returns the round point builder
-------------------------------------
Getter Method
Signature
RoundPoint()
Returns: Return type: NXOpen.CAM.RoundPointBuilder
New in version NX5.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
RotaryPolarMoveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.