RotaryPolarMoveBuilderLockPlaneType Enumeration

NXOpen.CAM.RotaryPolarMoveBuilder.LockPlaneType is an alias for NXOpen.CAM.RotaryPolarMoveBuilderLockPlaneType

class NXOpen.CAM.RotaryPolarMoveBuilderLockPlaneType

Bases: object

the lock plane type

Enum Members

Enum Member Enum Member Description
Xy
XY-Plane
Yz
YZ-Plane
Zx
ZX-Plane
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.