ReliefCut Class

class NXOpen.CAM.ReliefCut

Bases: NXOpen.TaggedObject

Represents the relief cut

New in version NX7.5.0.

Properties

Property Description
Depth Returns or sets the relief cut depth
DepthUnit Returns or sets the relief cut depth unit
Distance Returns or sets the relief cut distance
DistanceUnit Returns or sets the relief cut distance unit
Mode Returns or sets the relief cut mode
Number Returns or sets the relief cut number
Tag Returns the Tag for this object.

Methods

Enumerations

ReliefCutDepthUnits Enumeration the relief cut depth unit options
ReliefCutDistanceUnits Enumeration the relief cut distance unit options
ReliefCutModes Enumeration the relief cut options

Property Detail

Depth

ReliefCut.Depth

Returns or sets the relief cut depth

-------------------------------------

Getter Method

Signature Depth()

Returns:the relief cut depth
Return type:float

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Depth(depth)

Parameters:depth (float) – the relief plunge depth

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)

DepthUnit

ReliefCut.DepthUnit

Returns or sets the relief cut depth unit

-------------------------------------

Getter Method

Signature DepthUnit()

Returns:the relief cut depth unit
Return type:NXOpen.CAM.ReliefCutDepthUnits

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DepthUnit(unit)

Parameters:unit (NXOpen.CAM.ReliefCutDepthUnits) – the relief cut depth unit

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)

Distance

ReliefCut.Distance

Returns or sets the relief cut distance

-------------------------------------

Getter Method

Signature Distance()

Returns:the relief cut distance
Return type:float

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Distance(distance)

Parameters:distance (float) – the relief plunge distance

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)

DistanceUnit

ReliefCut.DistanceUnit

Returns or sets the relief cut distance unit

-------------------------------------

Getter Method

Signature DistanceUnit()

Returns:the relief cut distance unit
Return type:NXOpen.CAM.ReliefCutDistanceUnits

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DistanceUnit(unit)

Parameters:unit (NXOpen.CAM.ReliefCutDistanceUnits) – the relief cut distance unit

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)

Mode

ReliefCut.Mode

Returns or sets the relief cut mode

-------------------------------------

Getter Method

Signature Mode()

Returns:the relief cut mode
Return type:NXOpen.CAM.ReliefCutModes

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Mode(reliefCutValue)

Parameters:reliefCutValue (NXOpen.CAM.ReliefCutModes) – the relief cut mode

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)

Number

ReliefCut.Number

Returns or sets the relief cut number

-------------------------------------

Getter Method

Signature Number()

Returns:the relief cut number
Return type:int

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Number(number)

Parameters:number (int) – the relief cut number

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)