ReliefCutDepthUnits Enumeration

NXOpen.CAM.ReliefCut.DepthUnits is an alias for NXOpen.CAM.ReliefCutDepthUnits

class NXOpen.CAM.ReliefCutDepthUnits

Bases: object

the relief cut depth unit options

New in version NX7.5.0.

Enum Members

Enum Member Enum Member Description
Length
Length
Percent
Percent
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.