ProjVecCiBuilder Class¶
-
class
NXOpen.CAM.
ProjVecCiBuilder
¶ Bases:
NXOpen.TaggedObject
Represents a tool axis ci Builder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
BackOffDistance | Returns the back off projection distance |
Point | Returns or sets the Point |
Tag | Returns the Tag for this object. |
Vector | Returns or sets the Vector |
Methods¶
Method | Description |
---|---|
GetDpmProjType | Get the Project Type @return the project type value |
SetDpmProjType | Set the Project Type |
Enumerations¶
ProjVecCiBuilderDpmProjTypes Enumeration | Available types for Project Vector |
Property Detail¶
BackOffDistance¶
-
ProjVecCiBuilder.
BackOffDistance
¶ Returns the back off projection distance
-------------------------------------
Getter Method
Signature
BackOffDistance()
Returns: Return type: NXOpen.CAM.InheritableToolDepBuilder
New in version NX10.0.3.
License requirements: cam_base (“CAM BASE”)
Point¶
-
ProjVecCiBuilder.
Point
¶ Returns or sets the Point
-------------------------------------
Getter Method
Signature
Point()
Returns: the Point Return type: NXOpen.Point
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Point(pointTag)
Parameters: pointTag ( NXOpen.Point
) – the PointNew in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
Vector¶
-
ProjVecCiBuilder.
Vector
¶ Returns or sets the Vector
-------------------------------------
Getter Method
Signature
Vector()
Returns: the Vector Return type: NXOpen.Direction
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Vector(vector)
Parameters: vector ( NXOpen.Direction
) – the VectorNew in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
GetDpmProjType¶
-
ProjVecCiBuilder.
GetDpmProjType
¶ Get the Project Type
Signature
GetDpmProjType()
Returns: the project type value Return type: NXOpen.CAM.ProjVecCiBuilderDpmProjTypes
New in version NX5.0.0.
License requirements: None.
SetDpmProjType¶
-
ProjVecCiBuilder.
SetDpmProjType
¶ Set the Project Type
Signature
SetDpmProjType(projType)
Parameters: projType ( NXOpen.CAM.ProjVecCiBuilderDpmProjTypes
) – the project type valueNew in version NX5.0.0.
License requirements: None.