ProjVecCiBuilderDpmProjTypes Enumeration

NXOpen.CAM.ProjVecCiBuilder.DpmProjTypes is an alias for NXOpen.CAM.ProjVecCiBuilderDpmProjTypes

class NXOpen.CAM.ProjVecCiBuilderDpmProjTypes

Bases: object

Available types for Project Vector

Enum Members

Enum Member Enum Member Description
ProjVecFixed
Specify Vector
ProjVecToolAxis
Tool Axis
ProjVecFromPoint
way from Point
ProjVecToPoint
Toward Point
ProjVecFromLine
Away from Line
ProjVecToLine
Toward Line
ProjVecNormToDrive
Normal to Drive
ProjVecToDrive
Toward Drive
ProjVecRuling
Swarf Ruling
ProjVecUserDefined
User Function
ProjVecToolAxisUp
Tool Axis up
ProjVecTotal
Total
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.