ProfileStrategy Class

class NXOpen.CAM.ProfileStrategy

Bases: NXOpen.TaggedObject

Represents profile strategy

New in version NX6.0.0.

Properties

Property Description
Tag Returns the Tag for this object.
Type Returns or sets the profile strategy

Methods

Enumerations

ProfileStrategyTypes Enumeration the profile strategy options

Property Detail

Type

ProfileStrategy.Type

Returns or sets the profile strategy

-------------------------------------

Getter Method

Signature Type()

Returns:the profile strategy
Return type:NXOpen.CAM.ProfileStrategyTypes

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Type(type)

Parameters:type (NXOpen.CAM.ProfileStrategyTypes) – the profile strategy

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)