ProfileStrategyTypes Enumeration¶
NXOpen.CAM.ProfileStrategy.Types is an alias for NXOpen.CAM.ProfileStrategyTypes
-
class
NXOpen.CAM.
ProfileStrategyTypes
¶ Bases:
object
the profile strategy options
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description DiametersOnly Profile strategy: Diameters OnlyFacesOnly Profile strategy: Faces OnlyDiametersThenFaces Profile strategy: Diameters First, Then FacesFacesThenDiameters Profile strategy: Faces First, Then DiametersTowardsCorner Profile strategy: Towards CornerAwayFromCorner Profile strategy: Away from CornerDownOnly Profile strategy: Down OnlyFinishAll Profile strategy: Finish All-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-