ProbeParamsBuilder Class

class NXOpen.CAM.ProbeParamsBuilder

Bases: NXOpen.TaggedObject

Represents the Probe Params Builder

This builder cannot be instantiated separately.

New in version NX5.0.0.

Properties

Property Description
ProbeControlParameters Returns the probe control parameters builder
ProbeProtectedParameters Returns the probe protected parameters builder
ProbeStockParameters Returns the probe stock parameters builder
ProbeToleranceParameters Returns the probe tolerance parameters builder
Tag Returns the Tag for this object.

Methods

Property Detail

ProbeControlParameters

ProbeParamsBuilder.ProbeControlParameters

Returns the probe control parameters builder

-------------------------------------

Getter Method

Signature ProbeControlParameters()

Returns:
Return type:NXOpen.CAM.ProbeControlParametersBuilder

New in version NX5.0.0.

License requirements: None.

ProbeProtectedParameters

ProbeParamsBuilder.ProbeProtectedParameters

Returns the probe protected parameters builder

-------------------------------------

Getter Method

Signature ProbeProtectedParameters()

Returns:
Return type:NXOpen.CAM.ProbeProtectedParametersBuilder

New in version NX5.0.0.

License requirements: None.

ProbeStockParameters

ProbeParamsBuilder.ProbeStockParameters

Returns the probe stock parameters builder

-------------------------------------

Getter Method

Signature ProbeStockParameters()

Returns:
Return type:NXOpen.CAM.ProbeStockParametersBuilder

New in version NX5.0.0.

License requirements: None.

ProbeToleranceParameters

ProbeParamsBuilder.ProbeToleranceParameters

Returns the probe tolerance parameters builder

-------------------------------------

Getter Method

Signature ProbeToleranceParameters()

Returns:
Return type:NXOpen.CAM.ProbeToleranceParametersBuilder

New in version NX5.0.0.

License requirements: None.