ProbeCalibrateSphereMoveBuilder Class¶
-
class
NXOpen.CAM.
ProbeCalibrateSphereMoveBuilder
¶ Bases:
NXOpen.CAM.MoveBuilder
Represents the Probe Calibrate Sphere Move Builder
To create a new instance of this class, use
NXOpen.CAM.MoveCollection.CreateProbeCalibrateSphereMoveBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Diameter | Returns or sets the diameter defining the sphere to probe |
FeedRate | Returns or sets the feed rate |
FeedType | Returns or sets the feed type |
FeedUnit | Returns or sets the feed unit |
GeometryType | Returns or sets the type of geometry |
MotionType | Returns or sets the motion type |
NumberOfUserParameters | Returns the number of user parameters |
Point | Returns or sets the point defining the sphere to probe |
ProbeProtectedParameters | Returns the probe protected parameters builder |
ProtectedMove | Returns or sets the protected move status |
Sphere | Returns or sets the sphere to probe |
SubopLabel | Returns or sets the subop label |
Tag | Returns the Tag for this object. |
ToolOffset | Returns or sets the tool offset to update |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetUserParameter | Returns the custom parameter with the given name. |
SetParent | Set parent |
SetSibling | Set sibling |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ProbeCalibrateSphereMoveBuilderGeometry Enumeration | the geometry types |
Property Detail¶
Diameter¶
-
ProbeCalibrateSphereMoveBuilder.
Diameter
¶ Returns or sets the diameter defining the sphere to probe
-------------------------------------
Getter Method
Signature
Diameter()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Diameter(diameter)
Parameters: diameter (float) – New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
GeometryType¶
-
ProbeCalibrateSphereMoveBuilder.
GeometryType
¶ Returns or sets the type of geometry
-------------------------------------
Getter Method
Signature
GeometryType()
Returns: Return type: NXOpen.CAM.ProbeCalibrateSphereMoveBuilderGeometry
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GeometryType(geomType)
Parameters: geomType ( NXOpen.CAM.ProbeCalibrateSphereMoveBuilderGeometry
) –New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
Point¶
-
ProbeCalibrateSphereMoveBuilder.
Point
¶ Returns or sets the point defining the sphere to probe
-------------------------------------
Getter Method
Signature
Point()
Returns: Return type: NXOpen.Point
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Point(point)
Parameters: point ( NXOpen.Point
) –New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
ProbeProtectedParameters¶
-
ProbeCalibrateSphereMoveBuilder.
ProbeProtectedParameters
¶ Returns the probe protected parameters builder
-------------------------------------
Getter Method
Signature
ProbeProtectedParameters()
Returns: Return type: NXOpen.CAM.ProbeProtectedParametersBuilder
New in version NX5.0.0.
License requirements: None.
Sphere¶
-
ProbeCalibrateSphereMoveBuilder.
Sphere
¶ Returns or sets the sphere to probe
-------------------------------------
Getter Method
Signature
Sphere()
Returns: Return type: NXOpen.NXObject
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Sphere(sphere)
Parameters: sphere ( NXOpen.NXObject
) –New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
ToolOffset¶
-
ProbeCalibrateSphereMoveBuilder.
ToolOffset
¶ Returns or sets the tool offset to update
-------------------------------------
Getter Method
Signature
ToolOffset()
Returns: Return type: int New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolOffset(toolOffset)
Parameters: toolOffset (int) – New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
ProbeCalibrateSphereMoveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.