PostDebugBuilder Class¶
-
class
NXOpen.CAM.
PostDebugBuilder
¶ Bases:
NXOpen.Builder
Represents a
CAM.PostDebugBuilder
Use the
PostDebugBuilder
class to create a PostDebugBuilder object.New in version NX9.0.1.
Properties¶
Property | Description |
---|---|
DumpOutput | Returns or sets the dump output |
DumpToFileName | Returns or sets the output filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetTrace | Gets the trace @return The state |
SetTrace | Sets the trace |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
PostDebugBuilderOutputType Enumeration | The output type |
PostDebugBuilderTraceType Enumeration | Represents the trace type |
Property Detail¶
DumpOutput¶
-
PostDebugBuilder.
DumpOutput
¶ Returns or sets the dump output
-------------------------------------
Getter Method
Signature
DumpOutput()
Returns: The dump output type Return type: NXOpen.CAM.PostDebugBuilderOutputType
New in version NX9.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
DumpOutput(type)
Parameters: type ( NXOpen.CAM.PostDebugBuilderOutputType
) – The dump output typeNew in version NX9.0.1.
License requirements: cam_base (“CAM BASE”)
DumpToFileName¶
-
PostDebugBuilder.
DumpToFileName
¶ Returns or sets the output filename
-------------------------------------
Getter Method
Signature
DumpToFileName()
Returns: The output name Return type: str New in version NX9.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
DumpToFileName(name)
Parameters: name (str) – the output new name New in version NX9.0.1.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
GetTrace¶
-
PostDebugBuilder.
GetTrace
¶ Gets the trace
Signature
GetTrace(type)
Parameters: type ( NXOpen.CAM.PostDebugBuilderTraceType
) – The trace typeReturns: The state Return type: bool New in version NX9.0.1.
License requirements: None.
SetTrace¶
-
PostDebugBuilder.
SetTrace
¶ Sets the trace
Signature
SetTrace(type, state)
Parameters: - type (
NXOpen.CAM.PostDebugBuilderTraceType
) – The trace type - state (bool) – The state
New in version NX9.0.1.
License requirements: cam_base (“CAM BASE”)
- type (
Validate¶
-
PostDebugBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.