PostDebugBuilderTraceType Enumeration¶
NXOpen.CAM.PostDebugBuilder.TraceType is an alias for NXOpen.CAM.PostDebugBuilderTraceType
-
class
NXOpen.CAM.
PostDebugBuilderTraceType
¶ Bases:
object
Represents the trace type
Enum Members
Enum Member Enum Member Description OBuf Trace OutPut BufferDoEvent Trace DoEvent call in MOMDoEventFast Trace DoEventFast call in MOMTimer Trace timer when do post-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-