NcmClearanceBuilder Class¶
-
class
NXOpen.CAM.
NcmClearanceBuilder
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.CAM.NcmClearanceBuilder
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Axis | Returns or sets the clearance cylinder axis |
BoundingBoxClearance | Returns or sets the distance for bounding box clearance |
ClearanceType | Returns or sets the clearance type |
PlaneXform | Returns or sets the clearance plane,plane entity type covers Xform and Plane |
Point | Returns or sets the point for clearance types point, cylinder and sphere |
Radius | Returns or sets the clearance cylinder and sphere radius |
SafeDistance | Returns or sets the safe distance for automatic clearance |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
NcmClearanceBuilderClearanceTypes Enumeration | the types available for clearance |
Property Detail¶
Axis¶
-
NcmClearanceBuilder.
Axis
¶ Returns or sets the clearance cylinder axis
-------------------------------------
Getter Method
Signature
Axis()
Returns: Return type: NXOpen.NXObject
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Axis(axis)
Parameters: axis ( NXOpen.NXObject
) –New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
BoundingBoxClearance¶
-
NcmClearanceBuilder.
BoundingBoxClearance
¶ Returns or sets the distance for bounding box clearance
-------------------------------------
Getter Method
Signature
BoundingBoxClearance()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
BoundingBoxClearance(boundingBoxClearance)
Parameters: boundingBoxClearance (float) – New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
ClearanceType¶
-
NcmClearanceBuilder.
ClearanceType
¶ Returns or sets the clearance type
-------------------------------------
Getter Method
Signature
ClearanceType()
Returns: Return type: NXOpen.CAM.NcmClearanceBuilderClearanceTypes
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ClearanceType(clearanceType)
Parameters: clearanceType ( NXOpen.CAM.NcmClearanceBuilderClearanceTypes
) –New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
PlaneXform¶
-
NcmClearanceBuilder.
PlaneXform
¶ Returns or sets the clearance plane,plane entity type covers Xform and Plane
-------------------------------------
Getter Method
Signature
PlaneXform()
Returns: entity type can be XFORM or PLANE Return type: NXOpen.NXObject
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlaneXform(plane)
Parameters: plane ( NXOpen.NXObject
) – entity type can be XFORM or PLANENew in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
Point¶
-
NcmClearanceBuilder.
Point
¶ Returns or sets the point for clearance types point, cylinder and sphere
-------------------------------------
Getter Method
Signature
Point()
Returns: Return type: NXOpen.NXObject
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Point(point)
Parameters: point ( NXOpen.NXObject
) –New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
Radius¶
-
NcmClearanceBuilder.
Radius
¶ Returns or sets the clearance cylinder and sphere radius
-------------------------------------
Getter Method
Signature
Radius()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Radius(radius)
Parameters: radius (float) – New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
SafeDistance¶
-
NcmClearanceBuilder.
SafeDistance
¶ Returns or sets the safe distance for automatic clearance
-------------------------------------
Getter Method
Signature
SafeDistance()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SafeDistance(newValue)
Parameters: newValue (float) – New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)