NcmClearanceBuilderClearanceTypes Enumeration¶
NXOpen.CAM.NcmClearanceBuilder.ClearanceTypes is an alias for NXOpen.CAM.NcmClearanceBuilderClearanceTypes
-
class
NXOpen.CAM.
NcmClearanceBuilderClearanceTypes
¶ Bases:
object
the types available for clearance
Enum Members
Enum Member Enum Member Description UseCommon inherited from common or parentNotSet clearance turned offAutomatic automatic with distance for planar operationsPlane clearance planePoint clearance pointCylinder clearance cylinderSphere clearance sphereBoundingBox clearance boxBoundingCylinder clearance bounding cylinder-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-