ManualControlBuilder Class¶
-
class
NXOpen.CAM.
ManualControlBuilder
¶ Bases:
NXOpen.CAM.OperationBuilder
Represents a ManualControl Operation Builder
To create a new instance of this class, use
NXOpen.CAM.OperationCollection.CreateManualControlBuilder()
New in version NX10.0.3.
Properties¶
Property | Description |
---|---|
ChannelName | Returns or sets the channel’s name |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndOfPath | Returns the end event builder |
EndUdeSet | Returns the end ude set |
Geometry | Returns the geometry builder |
GougeChecking | Returns or sets the gouge checking flag |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
LayoutAndLayer | Returns the Layer and Layout |
MotionOutputBuilder | Returns the motion output builder |
Notes | Returns the notes builder |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
PathDisplayOptions | Returns the path display options builder |
PostToolPathExit | Returns or sets the environment variable that points to the post tool path generation library which has the exit |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
SafeClearance | Returns the safe clearance builder |
SelectToolFlag | Returns or sets the user selected tool |
StartOfPath | Returns the start event builder |
StartUdeSet | Returns the start ude set |
StopActive | Returns or sets the stop command status mode |
Tag | Returns the Tag for this object. |
ToolChangeSetting | Returns the tool change builder |
ToolPathEditor | Returns the Tool Path Editor Builder |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetHoleAxisValues | Get the Hole Axis values @return the Hole Axis values |
GetObject | Returns the object currently being edited by this builder. |
GetOperatorMessage | Returns the operator message @return |
SetHoleAxisValues | Set the Hole Axis values |
SetOperatorMessage | Sets the operator message |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
StopActive¶
-
ManualControlBuilder.
StopActive
¶ Returns or sets the stop command status mode
-------------------------------------
Getter Method
Signature
StopActive()
Returns: Return type: bool New in version NX10.0.3.
License requirements: None.
-------------------------------------
Setter Method
Signature
StopActive(status)
Parameters: status (bool) – New in version NX10.0.3.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
GetOperatorMessage¶
-
ManualControlBuilder.
GetOperatorMessage
¶ Returns the operator message
Signature
GetOperatorMessage()
Returns: Return type: list of str New in version NX10.0.3.
License requirements: None.
SetOperatorMessage¶
-
ManualControlBuilder.
SetOperatorMessage
¶ Sets the operator message
Signature
SetOperatorMessage(multiLineText)
Parameters: multiLineText (list of str) – New in version NX10.0.3.
License requirements: cam_base (“CAM BASE”)
Validate¶
-
ManualControlBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.