LaserCutoutDefinition Class

class NXOpen.CAM.LaserCutoutDefinition

Bases: NXOpen.TaggedObject

Represents cutout definition settings for laser move

New in version NX9.0.0.

Properties

Property Description
Angle Returns or sets the Angle
CenterPoint Returns or sets the Center Point
CornerRadius Returns or sets the Corner Radius
CutoutDefType Returns or sets the Cutout Definition Type
CutoutSection Returns or sets the Cutout Section
Diameter Returns or sets the Diameter
Length Returns or sets the Length
Tag Returns the Tag for this object.
Width Returns or sets the Width
WrenchSize Returns or sets the Wrench Size

Methods

Enumerations

LaserCutoutDefinitionTypes Enumeration the Cutout Definition Type enum

Property Detail

Angle

LaserCutoutDefinition.Angle

Returns or sets the Angle

-------------------------------------

Getter Method

Signature Angle()

Returns:the angle value
Return type:float

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Angle(newValue)

Parameters:newValue (float) – the angle value

New in version NX9.0.0.

License requirements: cam_base (“CAM BASE”)

CenterPoint

LaserCutoutDefinition.CenterPoint

Returns or sets the Center Point

-------------------------------------

Getter Method

Signature CenterPoint()

Returns:the center point
Return type:NXOpen.Point

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CenterPoint(newValue)

Parameters:newValue (NXOpen.Point) – the center point

New in version NX9.0.0.

License requirements: cam_base (“CAM BASE”)

CornerRadius

LaserCutoutDefinition.CornerRadius

Returns or sets the Corner Radius

-------------------------------------

Getter Method

Signature CornerRadius()

Returns:the corner radius value
Return type:float

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CornerRadius(newValue)

Parameters:newValue (float) – the corner radius value

New in version NX9.0.0.

License requirements: cam_base (“CAM BASE”)

CutoutDefType

LaserCutoutDefinition.CutoutDefType

Returns or sets the Cutout Definition Type

-------------------------------------

Getter Method

Signature CutoutDefType()

Returns:the cutout def type
Return type:NXOpen.CAM.LaserCutoutDefinitionTypes

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CutoutDefType(type)

Parameters:type (NXOpen.CAM.LaserCutoutDefinitionTypes) – the cutout def type

New in version NX9.0.0.

License requirements: cam_base (“CAM BASE”)

CutoutSection

LaserCutoutDefinition.CutoutSection

Returns or sets the Cutout Section

-------------------------------------

Getter Method

Signature CutoutSection()

Returns:the Cutout Section
Return type:NXOpen.Section

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature CutoutSection(cutoutSection)

Parameters:cutoutSection (NXOpen.Section) – the Cutout Section

New in version NX9.0.0.

License requirements: cam_base (“CAM BASE”)

Diameter

LaserCutoutDefinition.Diameter

Returns or sets the Diameter

-------------------------------------

Getter Method

Signature Diameter()

Returns:the diameter value
Return type:float

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Diameter(newValue)

Parameters:newValue (float) – the diameter value

New in version NX9.0.0.

License requirements: cam_base (“CAM BASE”)

Length

LaserCutoutDefinition.Length

Returns or sets the Length

-------------------------------------

Getter Method

Signature Length()

Returns:the length value
Return type:float

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Length(newValue)

Parameters:newValue (float) – the length value

New in version NX9.0.0.

License requirements: cam_base (“CAM BASE”)

Width

LaserCutoutDefinition.Width

Returns or sets the Width

-------------------------------------

Getter Method

Signature Width()

Returns:the width value
Return type:float

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Width(newValue)

Parameters:newValue (float) – the width value

New in version NX9.0.0.

License requirements: cam_base (“CAM BASE”)

WrenchSize

LaserCutoutDefinition.WrenchSize

Returns or sets the Wrench Size

-------------------------------------

Getter Method

Signature WrenchSize()

Returns:the wrench size value
Return type:float

New in version NX9.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature WrenchSize(newValue)

Parameters:newValue (float) – the wrench size value

New in version NX9.0.0.

License requirements: cam_base (“CAM BASE”)