InspectionReferenceFeatureModeBuilder Class¶
-
class
NXOpen.CAM.
InspectionReferenceFeatureModeBuilder
¶ Bases:
NXOpen.CAM.InheritableBuilder
Represents a builder for an inheritable reference feature mode enum value
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
InheritanceStatus | Returns or sets the inheritance status |
Tag | Returns the Tag for this object. |
Value | Returns or sets the current reference feature mode |
Methods¶
Property Detail¶
Value¶
-
InspectionReferenceFeatureModeBuilder.
Value
¶ Returns or sets the current reference feature mode
-------------------------------------
Getter Method
Signature
Value()
Returns: the current reference feature mode Return type: NXOpen.CAM.InspectionMethodBuilderReferenceFeatureModeTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Value(itemValue)
Parameters: itemValue ( NXOpen.CAM.InspectionMethodBuilderReferenceFeatureModeTypes
) – the new reference feature modeNew in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)