InspectionPatternFeatureBuilder Class¶
-
class
NXOpen.CAM.
InspectionPatternFeatureBuilder
¶ Bases:
NXOpen.CAM.OperationBuilder
Represents a CMM Inspection Pattern Feature builder
To create a new instance of this class, use
NXOpen.CAM.InspectionOperationCollection.CreateInspectionPatternFeatureBuilder()
New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
ChannelName | Returns or sets the channel’s name |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndOfPath | Returns the end event builder |
EndUdeSet | Returns the end ude set |
FeatureFilter | Returns or sets the feature filter used to filter the list of available features |
Geometry | Returns the geometry builder |
GougeChecking | Returns or sets the gouge checking flag |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
LayoutAndLayer | Returns the Layer and Layout |
MotionOutputBuilder | Returns the motion output builder |
Name | Returns or sets the pattern feature name |
Notes | Returns the notes builder |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
PathDisplayOptions | Returns the path display options builder |
PostToolPathExit | Returns or sets the environment variable that points to the post tool path generation library which has the exit |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
SafeClearance | Returns the safe clearance builder |
SelectFeatures | Returns the select features button used to select features from the screen |
SelectToolFlag | Returns or sets the user selected tool |
StartOfPath | Returns the start event builder |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
ToolChangeSetting | Returns the tool change builder |
ToolPathEditor | Returns the Tool Path Editor Builder |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetHoleAxisValues | Get the Hole Axis values @return the Hole Axis values |
GetObject | Returns the object currently being edited by this builder. |
GetSubFeatures | Returns the current subfeatures. |
SetHoleAxisValues | Set the Hole Axis values |
SetSubFeatures | Sets the current subfeatures. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
InspectionPatternFeatureBuilderFeatureFilterTypes Enumeration | Filter for the list of available inspection features for inclusion in the pattern. |
Property Detail¶
FeatureFilter¶
-
InspectionPatternFeatureBuilder.
FeatureFilter
¶ Returns or sets the feature filter used to filter the list of available features
-------------------------------------
Getter Method
Signature
FeatureFilter()
Returns: Return type: NXOpen.CAM.InspectionPatternFeatureBuilderFeatureFilterTypes
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FeatureFilter(featureFilter)
Parameters: featureFilter ( NXOpen.CAM.InspectionPatternFeatureBuilderFeatureFilterTypes
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Name¶
-
InspectionPatternFeatureBuilder.
Name
¶ Returns or sets the pattern feature name
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SelectFeatures¶
-
InspectionPatternFeatureBuilder.
SelectFeatures
¶ Returns the select features button used to select features from the screen
-------------------------------------
Getter Method
Signature
SelectFeatures()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX7.0.0.
License requirements: None.
Method Detail¶
GetSubFeatures¶
-
InspectionPatternFeatureBuilder.
GetSubFeatures
¶ Returns the current subfeatures.
Signature
GetSubFeatures()
Returns: Current subfeatures Return type: list of str New in version NX7.5.3.
License requirements: None.
SetSubFeatures¶
-
InspectionPatternFeatureBuilder.
SetSubFeatures
¶ Sets the current subfeatures.
Signature
SetSubFeatures(subFeatures)
Parameters: subFeatures (list of str) – Current subfeatures New in version NX7.5.3.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Validate¶
-
InspectionPatternFeatureBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.