InspectionCurveFeatureBuilder Class¶
-
class
NXOpen.CAM.
InspectionCurveFeatureBuilder
¶ Bases:
NXOpen.CAM.OperationBuilder
Represents a CMM Inspection Curve Feature builder
To create a new instance of this class, use
NXOpen.CAM.InspectionOperationCollection.CreateInspectionCurveFeatureBuilder()
New in version NX7.0.0.
Properties¶
Property | Description |
---|---|
ApproachDirection | Returns or sets the approach direction |
ChannelName | Returns or sets the channel’s name |
CurvatureFactor | Returns or sets the curvature factor |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndDistance | Returns or sets the end distance |
EndOfPath | Returns the end event builder |
EndPercentage | Returns or sets the end percentage |
EndUdeSet | Returns the end ude set |
Geometry | Returns the geometry builder |
GougeChecking | Returns or sets the gouge checking flag |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
IsPointDefinitionChanged | Returns or sets the point data definition changed flag |
LayoutAndLayer | Returns the Layer and Layout |
MaximumSpacing | Returns or sets the maximum spacing |
MinimumNumberOfPoints | Returns or sets the minimum number of points |
MinimumSpacing | Returns or sets the minimum spacing |
MotionOutputBuilder | Returns the motion output builder |
Name | Returns or sets the name |
Notes | Returns the notes builder |
OffsetDistance | Returns the offset distance |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
PathDisplayOptions | Returns the path display options builder |
PointDataDefinition | Returns or sets the point data definition |
PointSelector | Returns the user specified point selector |
PostToolPathExit | Returns or sets the environment variable that points to the post tool path generation library which has the exit |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
SafeClearance | Returns the safe clearance builder |
SelectToolFlag | Returns or sets the user selected tool |
SelectedCurves | Returns the selected curves |
SelectedSurfaces | Returns the underlying surfaces selector. |
StartDistance | Returns or sets the start distance |
StartEndMode | Returns or sets the start end mode |
StartOfPath | Returns the start event builder |
StartPercentage | Returns or sets the start percentage |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
ToolChangeSetting | Returns the tool change builder |
ToolPathEditor | Returns the Tool Path Editor Builder |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
ErasePointDefinitionDisplay | Erases display of point definition data |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetHoleAxisValues | Get the Hole Axis values @return the Hole Axis values |
GetObject | Returns the object currently being edited by this builder. |
PreviewPointData | Creates preview of point definition data |
ReverseFeatureNormal | Reverses the feature normal |
ReverseOffsetDirection | Reverses the offset direction |
SetHoleAxisValues | Set the Hole Axis values |
SetSelectedSurfaces | Sets the curve underlying selected surfaces |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UpdateOffset | Updates curve inspection feature characteristic parameters based on offset distance |
UpdateParams | Updates the feature parameters |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
InspectionCurveFeatureBuilderPointDataDefinitionType Enumeration | The method used to define point data |
InspectionCurveFeatureBuilderStartEndModeType Enumeration | the method used to define the start and end points |
Property Detail¶
ApproachDirection¶
-
InspectionCurveFeatureBuilder.
ApproachDirection
¶ Returns or sets the approach direction
-------------------------------------
Getter Method
Signature
ApproachDirection()
Returns: Return type: NXOpen.Direction
New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ApproachDirection(approachDirection)
Parameters: approachDirection ( NXOpen.Direction
) –New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
CurvatureFactor¶
-
InspectionCurveFeatureBuilder.
CurvatureFactor
¶ Returns or sets the curvature factor
-------------------------------------
Getter Method
Signature
CurvatureFactor()
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
CurvatureFactor(curvatureFactor)
Parameters: curvatureFactor (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EndDistance¶
-
InspectionCurveFeatureBuilder.
EndDistance
¶ Returns or sets the end distance
-------------------------------------
Getter Method
Signature
EndDistance()
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndDistance(endDistance)
Parameters: endDistance (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
EndPercentage¶
-
InspectionCurveFeatureBuilder.
EndPercentage
¶ Returns or sets the end percentage
-------------------------------------
Getter Method
Signature
EndPercentage()
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndPercentage(endPercentage)
Parameters: endPercentage (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
IsPointDefinitionChanged¶
-
InspectionCurveFeatureBuilder.
IsPointDefinitionChanged
¶ Returns or sets the point data definition changed flag
-------------------------------------
Getter Method
Signature
IsPointDefinitionChanged()
Returns: Return type: bool New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsPointDefinitionChanged(isChanged)
Parameters: isChanged (bool) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
MaximumSpacing¶
-
InspectionCurveFeatureBuilder.
MaximumSpacing
¶ Returns or sets the maximum spacing
-------------------------------------
Getter Method
Signature
MaximumSpacing()
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
MaximumSpacing(maximumSpacing)
Parameters: maximumSpacing (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
MinimumNumberOfPoints¶
-
InspectionCurveFeatureBuilder.
MinimumNumberOfPoints
¶ Returns or sets the minimum number of points
-------------------------------------
Getter Method
Signature
MinimumNumberOfPoints()
Returns: Return type: int New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
MinimumNumberOfPoints(minimumNumberOfPoints)
Parameters: minimumNumberOfPoints (int) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
MinimumSpacing¶
-
InspectionCurveFeatureBuilder.
MinimumSpacing
¶ Returns or sets the minimum spacing
-------------------------------------
Getter Method
Signature
MinimumSpacing()
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
MinimumSpacing(minimumSpacing)
Parameters: minimumSpacing (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Name¶
-
InspectionCurveFeatureBuilder.
Name
¶ Returns or sets the name
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX7.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Name(name)
Parameters: name (str) – New in version NX7.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
OffsetDistance¶
-
InspectionCurveFeatureBuilder.
OffsetDistance
¶ Returns the offset distance
-------------------------------------
Getter Method
Signature
OffsetDistance()
Returns: Return type: NXOpen.CAM.InheritableDoubleBuilder
New in version NX9.0.0.
License requirements: None.
PointDataDefinition¶
-
InspectionCurveFeatureBuilder.
PointDataDefinition
¶ Returns or sets the point data definition
-------------------------------------
Getter Method
Signature
PointDataDefinition()
Returns: Return type: NXOpen.CAM.InspectionCurveFeatureBuilderPointDataDefinitionType
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
PointDataDefinition(pointDataDefinition)
Parameters: pointDataDefinition ( NXOpen.CAM.InspectionCurveFeatureBuilderPointDataDefinitionType
) –New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PointSelector¶
-
InspectionCurveFeatureBuilder.
PointSelector
¶ Returns the user specified point selector
-------------------------------------
Getter Method
Signature
PointSelector()
Returns: Return type: NXOpen.SelectPointList
New in version NX8.5.1.
License requirements: None.
SelectedCurves¶
-
InspectionCurveFeatureBuilder.
SelectedCurves
¶ Returns the selected curves
-------------------------------------
Getter Method
Signature
SelectedCurves()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX7.0.0.
License requirements: None.
SelectedSurfaces¶
-
InspectionCurveFeatureBuilder.
SelectedSurfaces
¶ Returns the underlying surfaces selector.
-------------------------------------
Getter Method
Signature
SelectedSurfaces()
Returns: Return type: NXOpen.SelectNXObjectList
New in version NX7.0.0.
License requirements: None.
StartDistance¶
-
InspectionCurveFeatureBuilder.
StartDistance
¶ Returns or sets the start distance
-------------------------------------
Getter Method
Signature
StartDistance()
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartDistance(startDistance)
Parameters: startDistance (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StartEndMode¶
-
InspectionCurveFeatureBuilder.
StartEndMode
¶ Returns or sets the start end mode
-------------------------------------
Getter Method
Signature
StartEndMode()
Returns: Return type: NXOpen.CAM.InspectionCurveFeatureBuilderStartEndModeType
New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartEndMode(startEndMode)
Parameters: startEndMode ( NXOpen.CAM.InspectionCurveFeatureBuilderStartEndModeType
) –New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
StartPercentage¶
-
InspectionCurveFeatureBuilder.
StartPercentage
¶ Returns or sets the start percentage
-------------------------------------
Getter Method
Signature
StartPercentage()
Returns: Return type: float New in version NX8.5.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
StartPercentage(startPercentage)
Parameters: startPercentage (float) – New in version NX8.5.1.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Method Detail¶
ErasePointDefinitionDisplay¶
-
InspectionCurveFeatureBuilder.
ErasePointDefinitionDisplay
¶ Erases display of point definition data
Signature
ErasePointDefinitionDisplay()
New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
PreviewPointData¶
-
InspectionCurveFeatureBuilder.
PreviewPointData
¶ Creates preview of point definition data
Signature
PreviewPointData(showExisting)
Parameters: showExisting (bool) – New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ReverseFeatureNormal¶
-
InspectionCurveFeatureBuilder.
ReverseFeatureNormal
¶ Reverses the feature normal
Signature
ReverseFeatureNormal()
New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
ReverseOffsetDirection¶
-
InspectionCurveFeatureBuilder.
ReverseOffsetDirection
¶ Reverses the offset direction
Signature
ReverseOffsetDirection()
New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
SetSelectedSurfaces¶
-
InspectionCurveFeatureBuilder.
SetSelectedSurfaces
¶ Sets the curve underlying selected surfaces
Signature
SetSelectedSurfaces(selectedSurfaces)
Parameters: selectedSurfaces (list of NXOpen.Face
) – Array of selected surfacesNew in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UpdateOffset¶
-
InspectionCurveFeatureBuilder.
UpdateOffset
¶ Updates curve inspection feature characteristic parameters based on offset distance
Signature
UpdateOffset()
New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
UpdateParams¶
-
InspectionCurveFeatureBuilder.
UpdateParams
¶ Updates the feature parameters
Signature
UpdateParams()
New in version NX9.0.0.
License requirements: insp_programming (“INSPECTION PROGRAMMING”)
Validate¶
-
InspectionCurveFeatureBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.