InheritableTextBuilder Class

class NXOpen.CAM.InheritableTextBuilder

Bases: NXOpen.CAM.InheritableBuilder

Represents a builder for an inheritable text value in of a CAM.

CAMObject .. versionadded:: NX5.0.0

Properties

Property Description
InheritanceStatus Returns or sets the inheritance status
Tag Returns the Tag for this object.
Value Returns or sets the current value

Methods

Property Detail

Value

InheritableTextBuilder.Value

Returns or sets the current value

-------------------------------------

Getter Method

Signature Value()

Returns:the current value
Return type:str

New in version NX5.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Value(newValue)

Parameters:newValue (str) – the new value

New in version NX5.0.0.

License requirements: cam_base (“CAM BASE”)