InheritableBoolBuilder Class

class NXOpen.CAM.InheritableBoolBuilder

Bases: NXOpen.CAM.InheritableBuilder

Represents a builder for an inheritable integer value in of a CAM.

CAMObject .. versionadded:: NX8.5.3

Properties

Property Description
InheritanceStatus Returns or sets the inheritance status
Tag Returns the Tag for this object.
Value Returns or sets the current value

Methods

Property Detail

Value

InheritableBoolBuilder.Value

Returns or sets the current value

-------------------------------------

Getter Method

Signature Value()

Returns:the current value
Return type:bool

New in version NX8.5.3.

License requirements: None.

-------------------------------------

Setter Method

Signature Value(newValue)

Parameters:newValue (bool) – the new value

New in version NX8.5.3.

License requirements: cam_base (“CAM BASE”)