FeatureBasedGeomBuilder Class¶
-
class
NXOpen.CAM.
FeatureBasedGeomBuilder
¶ Bases:
NXOpen.CAM.FeatureGeomBuilder
Represents a FeatureBasedGeom Builder
To create a new instance of this class, use
NXOpen.CAM.NCGroupCollection.CreateFeatureBasedGeomBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
BlankOffsetBuilder | Returns the blank offset (inheritable double) |
CheckOffsetBuilder | Returns the check offset (inheritable double) |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
EndUdeSet | Returns the end ude set |
GeometryCiBuilder | Returns the geometry builder |
LayoutCiBuilder | Returns the save/layer layout builder |
OptimizationMethod | Returns or sets the optim method |
PartMaterialBuilder | Returns or sets the part material |
PartOffsetBuilder | Returns the part offset (inheritable double) |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
TrimOffsetBuilder | Returns the trim offset (inheritable double) |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetGeomParentStringValue | Get the string value of the geom parent parameter index from the object @return the string value |
GetMaterial | Get part material @return |
GetMaterialData | Get material data |
GetObject | Returns the object currently being edited by this builder. |
SetGeomParentStringValue | Set a string value to the geom parent parameter index for the object. |
SetMaterial | Set part material |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
GetGeomParentStringValue¶
-
FeatureBasedGeomBuilder.
GetGeomParentStringValue
¶ Get the string value of the geom parent parameter index from the object
Signature
GetGeomParentStringValue()
Returns: the string value Return type: str New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
SetGeomParentStringValue¶
-
FeatureBasedGeomBuilder.
SetGeomParentStringValue
¶ Set a string value to the geom parent parameter index for the object.
Signature
SetGeomParentStringValue(value)
Parameters: value (str) – the string value New in version NX5.0.0.
License requirements: cam_base (“CAM BASE”)
Validate¶
-
FeatureBasedGeomBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.