DmToolPosition Class¶
-
class
NXOpen.CAM.
DmToolPosition
¶ Bases:
NXOpen.TaggedObject
Represents a streamline tool position builder
This is an abstract class and cannot be instantiated.
New in version NX10.0.1.
Properties¶
Property | Description |
---|---|
Tag | Returns the Tag for this object. |
ToolPosition | Returns or sets the tool position |
Methods¶
Property Detail¶
ToolPosition¶
-
DmToolPosition.
ToolPosition
¶ Returns or sets the tool position
-------------------------------------
Getter Method
Signature
ToolPosition()
Returns: the tool position value Return type: NXOpen.CAM.DPMItpBuilderToolPositionOption
New in version NX10.0.1.
License requirements: None.
-------------------------------------
Setter Method
Signature
ToolPosition(toolPosition)
Parameters: toolPosition ( NXOpen.CAM.DPMItpBuilderToolPositionOption
) – the tool position valueNew in version NX10.0.1.
License requirements: cam_base (“CAM BASE”)