DPMItpBuilderToolPositionOption Enumeration

NXOpen.CAM.DPMItpBuilder.ToolPositionOption is an alias for NXOpen.CAM.DPMItpBuilderToolPositionOption

class NXOpen.CAM.DPMItpBuilderToolPositionOption

Bases: object

Enum of tool position

Enum Members

Enum Member Enum Member Description
On
On position
Tanto
Tanto position
Contact
Contact position
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.