DmSpiralBuilder Class

class NXOpen.CAM.DmSpiralBuilder

Bases: NXOpen.TaggedObject

Represents a Spiral Drive Method Builder

This is an abstract class and cannot be instantiated.

New in version NX5.0.0.

Properties

Property Description
DmSpiralStepoverMenu Returns or sets the Spiral Drive Method Stepover type.
PatternCenterPoint Returns or sets the Pattern Center Point
SpiralRadiusBuilder Returns the Spiral Radius
SpiralStepoverBuilder Returns the Spiral Stepover builder
SpiralStepoverDistance Returns or sets the Stepover Distance.
SpiralStepoverPercent Returns or sets the Stepover Percent.
Tag Returns the Tag for this object.

Methods

Enumerations

DmSpiralBuilderDmSpiralStepoverTypes Enumeration Available types for Spiral drive method stepover in SurfaceContour.

Property Detail

DmSpiralStepoverMenu

DmSpiralBuilder.DmSpiralStepoverMenu

Returns or sets the Spiral Drive Method Stepover type.

This property is obsolete.

-------------------------------------

Getter Method

Signature DmSpiralStepoverMenu()

Returns:the Spiral Stepover type value
Return type:NXOpen.CAM.DmSpiralBuilderDmSpiralStepoverTypes

New in version NX5.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature DmSpiralStepoverMenu(dmSpiralStepoverTypeValue)

Parameters:dmSpiralStepoverTypeValue (NXOpen.CAM.DmSpiralBuilderDmSpiralStepoverTypes) – the Spiral Stepover type value

New in version NX5.0.0.

License requirements: None.

PatternCenterPoint

DmSpiralBuilder.PatternCenterPoint

Returns or sets the Pattern Center Point

-------------------------------------

Getter Method

Signature PatternCenterPoint()

Returns:
Return type:NXOpen.Point

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature PatternCenterPoint(centerPoint)

Parameters:centerPoint (NXOpen.Point) –

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

SpiralRadiusBuilder

DmSpiralBuilder.SpiralRadiusBuilder

Returns the Spiral Radius

-------------------------------------

Getter Method

Signature SpiralRadiusBuilder()

Returns:the spiral radius value
Return type:NXOpen.CAM.InheritableDoubleBuilder

New in version NX5.0.0.

License requirements: None.

SpiralStepoverBuilder

DmSpiralBuilder.SpiralStepoverBuilder

Returns the Spiral Stepover builder

-------------------------------------

Getter Method

Signature SpiralStepoverBuilder()

Returns:the spiral stepover builder
Return type:NXOpen.CAM.StepoverBuilder

New in version NX6.0.0.

License requirements: None.

SpiralStepoverDistance

DmSpiralBuilder.SpiralStepoverDistance

Returns or sets the Stepover Distance.

This property is obsolete.

-------------------------------------

Getter Method

Signature SpiralStepoverDistance()

Returns:the Stepover Distance
Return type:float

New in version NX5.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature SpiralStepoverDistance(stepoverDist)

Parameters:stepoverDist (float) – the Stepover Distance

New in version NX5.0.0.

License requirements: None.

SpiralStepoverPercent

DmSpiralBuilder.SpiralStepoverPercent

Returns or sets the Stepover Percent.

This property is obsolete.

-------------------------------------

Getter Method

Signature SpiralStepoverPercent()

Returns:the Stepover Percent
Return type:float

New in version NX5.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature SpiralStepoverPercent(stepoverPercent)

Parameters:stepoverPercent (float) – the Stepover Percent

New in version NX5.0.0.

License requirements: None.