DmSpiralBuilderDmSpiralStepoverTypes Enumeration

NXOpen.CAM.DmSpiralBuilder.DmSpiralStepoverTypes is an alias for NXOpen.CAM.DmSpiralBuilderDmSpiralStepoverTypes

class NXOpen.CAM.DmSpiralBuilderDmSpiralStepoverTypes

Bases: object

Available types for Spiral drive method stepover in SurfaceContour.

This enum type is obsolete.

Enum Members

Enum Member Enum Member Description
Constant
Constant
ToolDiameter
Tool diameter percentage
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.