BladeFinish Class

class NXOpen.CAM.BladeFinish

Bases: NXOpen.CAM.Blade

Represents a Blade Finish Drive Method Builder

New in version NX7.5.0.

Properties

Property Description
CutDirection Returns or sets the Cut Direction
CutPattern Returns the cut pattern builder
GeometryToFinish Returns the Geometry to Finish
LeadingEdge Returns the leading edge builder
SidesToCut Returns the Sides to Cut
StartPoint Returns the Start Point
Tag Returns the Tag for this object.
TrailingEdge Returns the trailing edge builder

Methods

Property Detail

GeometryToFinish

BladeFinish.GeometryToFinish

Returns the Geometry to Finish

-------------------------------------

Getter Method

Signature GeometryToFinish()

Returns:the Geometry to Finish
Return type:NXOpen.CAM.BladeFinishGeom

New in version NX7.5.0.

License requirements: None.

SidesToCut

BladeFinish.SidesToCut

Returns the Sides to Cut

-------------------------------------

Getter Method

Signature SidesToCut()

Returns:the Sides to Cut
Return type:NXOpen.CAM.CutSides

New in version NX7.5.0.

License requirements: None.

StartPoint

BladeFinish.StartPoint

Returns the Start Point

-------------------------------------

Getter Method

Signature StartPoint()

Returns:the Start Point
Return type:NXOpen.CAM.BladeStartPoint

New in version NX7.5.0.

License requirements: None.