BladeFinishGeom Class

class NXOpen.CAM.BladeFinishGeom

Bases: NXOpen.TaggedObject

Represents BladeFinishGeom Builder

New in version NX7.5.0.

Properties

Property Description
Tag Returns the Tag for this object.
Type Returns or sets the Geometry to Finish

Methods

Enumerations

BladeFinishGeomTypes Enumeration Available types for geometry to finish

Property Detail

Type

BladeFinishGeom.Type

Returns or sets the Geometry to Finish

-------------------------------------

Getter Method

Signature Type()

Returns:the Geometry to Finish value
Return type:NXOpen.CAM.BladeFinishGeomTypes

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature Type(geomToFinish)

Parameters:geomToFinish (NXOpen.CAM.BladeFinishGeomTypes) – the Geometry to Finish value

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)