ArcOutputTypeCiBuilder Class

class NXOpen.CAM.ArcOutputTypeCiBuilder

Bases: NXOpen.TaggedObject

Represents a ArcOutputTypeCiBuilder

New in version NX5.0.0.

Properties

Property Description
NurbAngleTolerance Returns or sets the nurb angle tolerance
NurbFitTolerance Returns or sets the nurb fit tolerance
NurbJoinSegments Returns or sets the nurb join segments
OutputType Returns or sets the Motion Output Type
SplineArcOutputType Returns or sets the spline arc output type
SplineFitTolerance Returns or sets the spline fit tolerance
SplineFitToleranceType Returns or sets the spline fit tolerance type
SplineLineOutputType Returns or sets the spline line output type
Tag Returns the Tag for this object.

Methods

Enumerations

ArcOutputTypeCiBuilderOutputTypes Enumeration Available types for output
ArcOutputTypeCiBuilderSplineArcOutputTypes Enumeration the available types for spline arc output
ArcOutputTypeCiBuilderSplineFitToleranceTypes Enumeration the available types for spline fitting tolerance
ArcOutputTypeCiBuilderSplineLineOutputTypes Enumeration the available types for spline line output

Property Detail

NurbAngleTolerance

ArcOutputTypeCiBuilder.NurbAngleTolerance

Returns or sets the nurb angle tolerance

-------------------------------------

Getter Method

Signature NurbAngleTolerance()

Returns:the nurb angle tolerance
Return type:float

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature NurbAngleTolerance(nurbsAngleTolerance)

Parameters:nurbsAngleTolerance (float) – the nurb angle tolerance

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)

NurbFitTolerance

ArcOutputTypeCiBuilder.NurbFitTolerance

Returns or sets the nurb fit tolerance

-------------------------------------

Getter Method

Signature NurbFitTolerance()

Returns:the nurb fit tolerance
Return type:float

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature NurbFitTolerance(nurbsFitTolerance)

Parameters:nurbsFitTolerance (float) – the nurb fit tolerance

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)

NurbJoinSegments

ArcOutputTypeCiBuilder.NurbJoinSegments

Returns or sets the nurb join segments

-------------------------------------

Getter Method

Signature NurbJoinSegments()

Returns:the nurb join segments
Return type:bool

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature NurbJoinSegments(nurbsJoinSegments)

Parameters:nurbsJoinSegments (bool) – the nurb join segments

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)

OutputType

ArcOutputTypeCiBuilder.OutputType

Returns or sets the Motion Output Type

-------------------------------------

Getter Method

Signature OutputType()

Returns:the motion output type
Return type:NXOpen.CAM.ArcOutputTypeCiBuilderOutputTypes

New in version NX5.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature OutputType(outputType)

Parameters:outputType (NXOpen.CAM.ArcOutputTypeCiBuilderOutputTypes) – the motion output type

New in version NX5.0.0.

License requirements: cam_base (“CAM BASE”)

SplineArcOutputType

ArcOutputTypeCiBuilder.SplineArcOutputType

Returns or sets the spline arc output type

-------------------------------------

Getter Method

Signature SplineArcOutputType()

Returns:the spline arc output type
Return type:NXOpen.CAM.ArcOutputTypeCiBuilderSplineArcOutputTypes

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature SplineArcOutputType(outputType)

Parameters:outputType (NXOpen.CAM.ArcOutputTypeCiBuilderSplineArcOutputTypes) – the spline arc output type

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)

SplineFitTolerance

ArcOutputTypeCiBuilder.SplineFitTolerance

Returns or sets the spline fit tolerance

-------------------------------------

Getter Method

Signature SplineFitTolerance()

Returns:the spline fit tolerance
Return type:float

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature SplineFitTolerance(splineFitTolerance)

Parameters:splineFitTolerance (float) – the spline fit tolerance

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)

SplineFitToleranceType

ArcOutputTypeCiBuilder.SplineFitToleranceType

Returns or sets the spline fit tolerance type

-------------------------------------

Getter Method

Signature SplineFitToleranceType()

Returns:the spline fit tolerance type
Return type:NXOpen.CAM.ArcOutputTypeCiBuilderSplineFitToleranceTypes

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature SplineFitToleranceType(outputType)

Parameters:outputType (NXOpen.CAM.ArcOutputTypeCiBuilderSplineFitToleranceTypes) – the spline fit tolerance type

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)

SplineLineOutputType

ArcOutputTypeCiBuilder.SplineLineOutputType

Returns or sets the spline line output type

-------------------------------------

Getter Method

Signature SplineLineOutputType()

Returns:the spline line output type
Return type:NXOpen.CAM.ArcOutputTypeCiBuilderSplineLineOutputTypes

New in version NX7.5.0.

License requirements: None.

-------------------------------------

Setter Method

Signature SplineLineOutputType(outputType)

Parameters:outputType (NXOpen.CAM.ArcOutputTypeCiBuilderSplineLineOutputTypes) – the spline line output type

New in version NX7.5.0.

License requirements: cam_base (“CAM BASE”)