ArcOutputTypeCiBuilderSplineLineOutputTypes Enumeration

NXOpen.CAM.ArcOutputTypeCiBuilder.SplineLineOutputTypes is an alias for NXOpen.CAM.ArcOutputTypeCiBuilderSplineLineOutputTypes

class NXOpen.CAM.ArcOutputTypeCiBuilderSplineLineOutputTypes

Bases: object

the available types for spline line output

Enum Members

Enum Member Enum Member Description
Spline
spline
Line
line
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.