GeneralDisplayStyles Class

class NXOpen.CAE.Xyplot.GeneralDisplayStyles

Bases: NXOpen.TaggedObject, NXOpen.CAE.Xyplot.IDisplayStyle

Manages the general display styles.

Not support KF.

New in version NX10.0.0.

Properties

Property Description
Owner Returns the owner style
PhaseAngle Returns or sets the phase angle in degree
PhaseRangeOption Returns or sets the phase range option
Tag Returns the Tag for this object.

Methods

Method Description
CommitChange Commits any edits that have been applied to the display style.

Property Detail

Owner

GeneralDisplayStyles.Owner

Returns the owner style

-------------------------------------

Getter Method

Signature Owner()

Returns:
Return type:NXOpen.CAE.Xyplot.IDisplayStyle

New in version NX10.0.0.

License requirements: None.

PhaseAngle

GeneralDisplayStyles.PhaseAngle

Returns or sets the phase angle in degree

-------------------------------------

Getter Method

Signature PhaseAngle()

Returns:Phase angle
Return type:float

New in version NX10.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature PhaseAngle(phaseAngle)

Parameters:phaseAngle (float) – Phase angle

New in version NX10.0.0.

License requirements: nx_ftk (“NX Advanced Graphing”)

PhaseRangeOption

GeneralDisplayStyles.PhaseRangeOption

Returns or sets the phase range option

-------------------------------------

Getter Method

Signature PhaseRangeOption()

Returns:Phase range option
Return type:NXOpen.CAE.Xyplot.PhaseRangeOption

New in version NX10.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature PhaseRangeOption(phaseRangeOption)

Parameters:phaseRangeOption (NXOpen.CAE.Xyplot.PhaseRangeOption) – Phase range option

New in version NX10.0.0.

License requirements: nx_ftk (“NX Advanced Graphing”)

Method Detail

CommitChange

GeneralDisplayStyles.CommitChange

Commits any edits that have been applied to the display style.

Triggers the corresponding plot to update graph.

Signature CommitChange()

New in version NX9.0.0.

License requirements: nx_ftk (“NX Advanced Graphing”)