PhaseRangeOption Enumeration¶
-
class
NXOpen.CAE.Xyplot.
PhaseRangeOption
¶ Bases:
object
Prepresents the phase range option Enum Members
Enum Member Enum Member Description NegativeTwoPiToZero Displays phase between -360 and 0ZeroToTwoPi Displays phase between 0 and 360NegativePiToPi Displays phase between -180 and 180NegativeOneHalfPiToHalfPi Displays phase between -270 and 90NegativeHalfPiToOneHalfPi Displays phase between -90 and 270-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-