SolutionBuilder Class¶
-
class
NXOpen.CAE.ResponseSimulation.
SolutionBuilder
¶ Bases:
NXOpen.CAE.ResponseSimulation.BaseBuilder
This is a manager to the
NXOpen.CAE.ResponseSimulation.Solution
class.Object of type
NXOpen.CAE.ResponseSimulation.Solution
can be created and edited only through this classTo create a new instance of this class, use
NXOpen.CAE.ResponseSimulation.SolutionCollection.CreateSolutionBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Attributes | Returns the attributes setting |
ImportedEefFile | Returns or sets the EEF file imported to create an imported response analysis meta solution. |
ObjectLabel | Returns the object label |
ReferencedSolution | Returns or sets the referenced solution which must be a SEMODES *103 solution with modal results solved |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Attributes¶
-
SolutionBuilder.
Attributes
¶ Returns the attributes setting
-------------------------------------
Getter Method
Signature
Attributes()
Returns: Return type: NXOpen.CAE.ResponseSimulation.SolutionAttributes
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
ImportedEefFile¶
-
SolutionBuilder.
ImportedEefFile
¶ Returns or sets the EEF file imported to create an imported response analysis meta solution.
There is event definition containing in the EEF file. An event will be created with the solution. To the imported solution and event, the users can only perform evaluation and not able to create new events and excitations
-------------------------------------
Getter Method
Signature
ImportedEefFile()
Returns: Return type: str New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
ImportedEefFile(importedEefFile)
Parameters: importedEefFile (str) – New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
ReferencedSolution¶
-
SolutionBuilder.
ReferencedSolution
¶ Returns or sets the referenced solution which must be a SEMODES *103 solution with modal results solved
-------------------------------------
Getter Method
Signature
ReferencedSolution()
Returns: Return type: NXOpen.CAE.SimSolution
New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
-------------------------------------
Setter Method
Signature
ReferencedSolution(referencedSolution)
Parameters: referencedSolution ( NXOpen.CAE.SimSolution
) – This parameter may not be None.New in version NX5.0.0.
License requirements: nx_response_anlys (“NX Response Analysis”)
Method Detail¶
Validate¶
-
SolutionBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.