TBSTopologyRestrictAreaBuilder Class¶
-
class
NXOpen.CAE.Optimization.
TBSTopologyRestrictAreaBuilder
¶ Bases:
NXOpen.CAE.Optimization.TBSRestrictAreaBuilder
Represents the builder of
NXOpen.CAE.Optimization.TBSTopologyRestrictArea
To create a new instance of this class, use
NXOpen.CAE.Optimization.TBSOptimizationManager.CreateTopologyRestrictAreaBuilder()
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
CastCondition | Returns the cast condition |
CheckingElementGroup | Returns the elements to react on the restrictions |
CheckingType | Returns or sets the checking type |
Distance | Returns the distance value |
LinkCondition | Returns the link condition |
MinimumThickness | Returns the minimum thickness of the structure |
NameDescription | Returns the name description |
Radius | Returns the radius |
Tag | Returns the Tag for this object. |
Thickness | Returns the maximum thickness of the structure |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
TBSTopologyRestrictAreaBuilderCheckTypeOption Enumeration | Defines the type of restriction |
Property Detail¶
CastCondition¶
-
TBSTopologyRestrictAreaBuilder.
CastCondition
¶ Returns the cast condition
-------------------------------------
Getter Method
Signature
CastCondition()
Returns: Return type: NXOpen.CAE.Optimization.TBSCastCondition
New in version NX8.0.0.
License requirements: None.
CheckingElementGroup¶
-
TBSTopologyRestrictAreaBuilder.
CheckingElementGroup
¶ Returns the elements to react on the restrictions
-------------------------------------
Getter Method
Signature
CheckingElementGroup()
Returns: Return type: NXOpen.CAE.Optimization.TBSGroupDefinition
New in version NX8.0.0.
License requirements: None.
CheckingType¶
-
TBSTopologyRestrictAreaBuilder.
CheckingType
¶ Returns or sets the checking type
-------------------------------------
Getter Method
Signature
CheckingType()
Returns: Return type: NXOpen.CAE.Optimization.TBSTopologyRestrictAreaBuilderCheckTypeOption
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CheckingType(checkType)
Parameters: checkType ( NXOpen.CAE.Optimization.TBSTopologyRestrictAreaBuilderCheckTypeOption
) –New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
Distance¶
-
TBSTopologyRestrictAreaBuilder.
Distance
¶ Returns the distance value
-------------------------------------
Getter Method
Signature
Distance()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
LinkCondition¶
-
TBSTopologyRestrictAreaBuilder.
LinkCondition
¶ Returns the link condition
-------------------------------------
Getter Method
Signature
LinkCondition()
Returns: Return type: NXOpen.CAE.Optimization.TBSTopologyLinkCondition
New in version NX8.0.0.
License requirements: None.
MinimumThickness¶
-
TBSTopologyRestrictAreaBuilder.
MinimumThickness
¶ Returns the minimum thickness of the structure
-------------------------------------
Getter Method
Signature
MinimumThickness()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
Radius¶
-
TBSTopologyRestrictAreaBuilder.
Radius
¶ Returns the radius
-------------------------------------
Getter Method
Signature
Radius()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
Thickness¶
-
TBSTopologyRestrictAreaBuilder.
Thickness
¶ Returns the maximum thickness of the structure
-------------------------------------
Getter Method
Signature
Thickness()
Returns: Return type: NXOpen.Expression
New in version NX8.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
TBSTopologyRestrictAreaBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.