TBSTopologyRestrictAreaBuilderCheckTypeOption Enumeration¶
NXOpen.CAE.Optimization.TBSTopologyRestrictAreaBuilder.CheckTypeOption is an alias for NXOpen.CAE.Optimization.TBSTopologyRestrictAreaBuilderCheckTypeOption
-
class
NXOpen.CAE.Optimization.
TBSTopologyRestrictAreaBuilderCheckTypeOption
¶ Bases:
object
Defines the type of restriction
Enum Members
- changes during optimization”
- “LinkTopo”, ” Definition of symmetry and link condtions ” “MaximumsSize”, ” Defition of the maximum structural diameter” “MinimumSize”, ” Definition of minimum structural diameter ” “Cast”, ” Manufacturing restrictions to guarantee the manufacturing of the elements”
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.