TBSLoadCaseManager Class¶
-
class
NXOpen.CAE.Optimization.
TBSLoadCaseManager
¶ Bases:
NXOpen.TaggedObject
Managers load cases
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
SelectionOption | Returns or sets the selection option |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AddLoadCases | Adds the load cases |
GetLoadCases | Returns the load cases @return |
RemoveLoadCases | Removes the load cases |
SetLoadCases | Sets the load cases |
Enumerations¶
TBSLoadCaseManagerSelectionType Enumeration | Defines the selection of the loadcase |
Property Detail¶
SelectionOption¶
-
TBSLoadCaseManager.
SelectionOption
¶ Returns or sets the selection option
-------------------------------------
Getter Method
Signature
SelectionOption()
Returns: Return type: NXOpen.CAE.Optimization.TBSLoadCaseManagerSelectionType
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SelectionOption(selectionOption)
Parameters: selectionOption ( NXOpen.CAE.Optimization.TBSLoadCaseManagerSelectionType
) –New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
Method Detail¶
AddLoadCases¶
-
TBSLoadCaseManager.
AddLoadCases
¶ Adds the load cases
Signature
AddLoadCases(loadCases)
Parameters: loadCases (list of NXOpen.CAE.Optimization.TBSLoadCase
) –New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
GetLoadCases¶
-
TBSLoadCaseManager.
GetLoadCases
¶ Returns the load cases
Signature
GetLoadCases()
Returns: Return type: list of NXOpen.CAE.Optimization.TBSLoadCase
New in version NX8.0.0.
License requirements: None.
RemoveLoadCases¶
-
TBSLoadCaseManager.
RemoveLoadCases
¶ Removes the load cases
Signature
RemoveLoadCases(loadCases, deleteLoadCase)
Parameters: - loadCases (list of
NXOpen.CAE.Optimization.TBSLoadCase
) – - deleteLoadCase (bool) –
New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)
- loadCases (list of
SetLoadCases¶
-
TBSLoadCaseManager.
SetLoadCases
¶ Sets the load cases
Signature
SetLoadCases(loadCases)
Parameters: loadCases (list of NXOpen.CAE.Optimization.TBSLoadCase
) –New in version NX8.0.0.
License requirements: cae_opt_topo (“NX Topology Optimization”) OR cae_opt_topobead (“NX Bead Optimization”) OR cae_opt_toposhape (“NX Shape Optimization”)