TBSLoadCaseManagerSelectionType Enumeration¶
NXOpen.CAE.Optimization.TBSLoadCaseManager.SelectionType is an alias for NXOpen.CAE.Optimization.TBSLoadCaseManagerSelectionType
-
class
NXOpen.CAE.Optimization.
TBSLoadCaseManagerSelectionType
¶ Bases:
object
Defines the selection of the loadcase
Enum Members
Enum Member Enum Member Description Maximum Maximum value of the selected load casesMinimum Minimum value of the selected load casesSum Sum of the selected load cases-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-