DAOObjective Class¶
-
class
NXOpen.CAE.Optimization.
DAOObjective
¶ Bases:
NXOpen.NXObject
Represents a
NXOpen.CAE.Optimization.DAOObjective
.New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
CategoryType | Returns or sets the category type |
GeometryType | Returns or sets the geometry type |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
LoadCase | Returns or sets the frequency load case index |
ModeNumber | Returns or sets the frequency mode number |
Name | Returns the custom name of the object. |
ObjectiveGoal | Returns or sets the objective goal |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Response | Returns or sets the objective response |
ResultMeasure | Returns or sets the result measure |
Tag | Returns the Tag for this object. |
TargetUnit | Returns or sets the target unit |
TargetValue | Returns or sets the target value |
Methods¶
Method | Description |
---|---|
CreateAttributeIterator | Create an attribute iterator @return A new attribute iterator object |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetGeometry | Gets the target geometry @return Target geometry |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetNumberResultGroup | Gets the objective result group number @return Result group number |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetResults | Gets the objective results @return Objective optimization results |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator @return |
Prints a representation of this object to the system log file. | |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetGeometry | Sets the target geometry |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
Property Detail¶
CategoryType¶
-
DAOObjective.
CategoryType
¶ Returns or sets the category type
-------------------------------------
Getter Method
Signature
CategoryType()
Returns: Category type Return type: NXOpen.CAE.Optimization.Category
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CategoryType(categoryType)
Parameters: categoryType ( NXOpen.CAE.Optimization.Category
) – Category typeNew in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
GeometryType¶
-
DAOObjective.
GeometryType
¶ Returns or sets the geometry type
-------------------------------------
Getter Method
Signature
GeometryType()
Returns: Geometry type Return type: NXOpen.CAE.Optimization.Geometry
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GeometryType(geometryType)
Parameters: geometryType ( NXOpen.CAE.Optimization.Geometry
) – Geometry typeNew in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
IsOccurrence¶
-
DAOObjective.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
DAOObjective.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
LoadCase¶
-
DAOObjective.
LoadCase
¶ Returns or sets the frequency load case index
-------------------------------------
Getter Method
Signature
LoadCase()
Returns: Return type: int New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LoadCase(loadcase)
Parameters: loadcase (int) – New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ModeNumber¶
-
DAOObjective.
ModeNumber
¶ Returns or sets the frequency mode number
-------------------------------------
Getter Method
Signature
ModeNumber()
Returns: Mode number Return type: int New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ModeNumber(modeNumber)
Parameters: modeNumber (int) – Mode number New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Name¶
-
DAOObjective.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
ObjectiveGoal¶
-
DAOObjective.
ObjectiveGoal
¶ Returns or sets the objective goal
-------------------------------------
Getter Method
Signature
ObjectiveGoal()
Returns: Objective goal Return type: NXOpen.CAE.Optimization.Goal
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ObjectiveGoal(objectiveGoal)
Parameters: objectiveGoal ( NXOpen.CAE.Optimization.Goal
) – Objective goalNew in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
OwningComponent¶
-
DAOObjective.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
DAOObjective.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
DAOObjective.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Response¶
-
DAOObjective.
Response
¶ Returns or sets the objective response
-------------------------------------
Getter Method
Signature
Response()
Returns: Objective response Return type: NXOpen.CAE.Optimization.Response
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Response(objectiveResponse)
Parameters: objectiveResponse ( NXOpen.CAE.Optimization.Response
) – Objective responseNew in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ResultMeasure¶
-
DAOObjective.
ResultMeasure
¶ Returns or sets the result measure
-------------------------------------
Getter Method
Signature
ResultMeasure()
Returns: Return type: NXOpen.CAE.ResultMeasure
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ResultMeasure(resMeas)
Parameters: resMeas ( NXOpen.CAE.ResultMeasure
) –New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
TargetUnit¶
-
DAOObjective.
TargetUnit
¶ Returns or sets the target unit
-------------------------------------
Getter Method
Signature
TargetUnit()
Returns: Target unit Return type: NXOpen.Unit
New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TargetUnit(targetUnit)
Parameters: targetUnit ( NXOpen.Unit
) – Target unitNew in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
TargetValue¶
-
DAOObjective.
TargetValue
¶ Returns or sets the target value
-------------------------------------
Getter Method
Signature
TargetValue()
Returns: Target value Return type: float New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TargetValue(targetValue)
Parameters: targetValue (float) – Target value New in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Method Detail¶
FindObject¶
-
DAOObjective.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetGeometry¶
-
DAOObjective.
GetGeometry
¶ Gets the target geometry
Signature
GetGeometry()
Returns: Target geometry Return type: list of NXOpen.DisplayableObject
New in version NX8.0.0.
License requirements: None.
GetNumberResultGroup¶
-
DAOObjective.
GetNumberResultGroup
¶ Gets the objective result group number
Signature
GetNumberResultGroup()
Returns: Result group number Return type: int New in version NX8.0.0.
License requirements: None.
GetResults¶
-
DAOObjective.
GetResults
¶ Gets the objective results
Signature
GetResults(resultGroupIndex)
Parameters: resultGroupIndex (int) – Result group index Returns: Objective optimization results Return type: list of float New in version NX8.0.0.
License requirements: None.
Print¶
-
DAOObjective.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetGeometry¶
-
DAOObjective.
SetGeometry
¶ Sets the target geometry
Signature
SetGeometry(geometry)
Parameters: geometry (list of NXOpen.DisplayableObject
) – Target geometryNew in version NX8.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SetName¶
-
DAOObjective.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.