Response Enumeration¶
-
class
NXOpen.CAE.Optimization.
Response
¶ Bases:
object
Represents the specific variable Enum Members
Enum Member Enum Member Description NotSet Weight Volume Frequency Temperature StressVonMises StrainVonMises TranslationX TranslationY TranslationZ RotationX RotationY RotationZ Stress2DMaximumShear Stress2DMajorPrincipal Stress2DMinorPrincipal Stress2DVonMises Stress2DMaximumShearBottom Stress2DMajorPrincipalBottom Stress2DMinorPrincipalBottom Stress2DVonMisesBottom Strain2DMaximumShear Strain2DMajorPrincipal Strain2DMinorPrincipal Strain2DVonMises Strain2DMaximumShearBottom Strain2DMajorPrincipalBottom Strain2DMinorPrincipalBottom Strain2DVonMisesBottom Stress1DVonMisesStressRecoveryPointC Stress1DVonMisesStressRecoveryPointD Stress1DVonMisesStressRecoveryPointE Stress1DVonMisesStressRecoveryPointF Stress1DVonMisesMaximum Stress1DVonMisesMinimum Strain1DVonMisesStressRecoveryPointC Strain1DVonMisesStressRecoveryPointD Strain1DVonMisesStressRecoveryPointE Strain1DVonMisesStressRecoveryPointF Strain1DVonMisesMaximum Strain1DVonMisesMinimum Stress3DFirstPrincipal Stress3DSecondPrincipal Stress3DThirdPrincipal Stress3DVonMises Strain3DFirstPrincipal Strain3DSecondPrincipal Strain3DThirdPrincipal Strain3DVonMises ResultMeasure Response type is a result measure-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-