TestResult Class

class NXOpen.CAE.ModelCheck.TestResult

Bases: NXOpen.TransientObject

Represents quality checking result of a quality test

To obtain an instance of this class use CAE.ModelCheck.ElementTestResult.GetTestResults

New in version NX8.5.0.

Properties

Property Description
TestType Returns the test type
TestValue Returns the test value.
ValidatedTestResult Returns the validation result of comparing test value with the criteria value.

Methods

Method Description
Dispose Frees the object from memory.
HasTestValue Tells whether there is a test value associated with this test @return

Property Detail

TestType

TestResult.TestType

Returns the test type

-------------------------------------

Getter Method

Signature TestType()

Returns:
Return type:NXOpen.CAE.ModelCheck.TestValueTypesTestType

New in version NX8.5.0.

License requirements: None.

TestValue

TestResult.TestValue

Returns the test value.

An exception will be thrown f there is no test value associated with this test

-------------------------------------

Getter Method

Signature TestValue()

Returns:
Return type:float

New in version NX8.5.0.

License requirements: None.

ValidatedTestResult

TestResult.ValidatedTestResult

Returns the validation result of comparing test value with the criteria value.

if no test value is associated this test, the result just indicates the test is passed or failed

-------------------------------------

Getter Method

Signature ValidatedTestResult()

Returns:
Return type:NXOpen.CAE.ModelCheck.TestValueTypesResult

New in version NX8.5.0.

License requirements: None.

Method Detail

Dispose

TestResult.Dispose

Frees the object from memory.

After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.

Signature Dispose()

New in version NX8.5.0.

License requirements: None.

HasTestValue

TestResult.HasTestValue

Tells whether there is a test value associated with this test

Signature HasTestValue()

Returns:
Return type:bool

New in version NX8.5.0.

License requirements: None.