TestValueTypesTestType Enumeration¶
NXOpen.CAE.ModelCheck.TestValueTypes.TestType is an alias for NXOpen.CAE.ModelCheck.TestValueTypesTestType
-
class
NXOpen.CAE.ModelCheck.
TestValueTypesTestType
¶ Bases:
object
the test types
Enum Members
check consistent Y. When elements are modeled in XY plane, check consistent Z.”
“AxisymmetricX”, ” When elements are modeled in XZ plane,check X >= 0.0. When elements are modeled in XY plane, check Y >= 0.0.”
“AspectRatio”, ” - ” “SkewAngle”, ” - ” “InteriorAngleMinimum”, ” - ” “InteriorAngleMaximum”, ” - ” “Taper”, ” - ” “WarpFactor”, ” - ” “FaceWarpCoefficient”, ” - ” “EdgePointLengthRatio”, ” - ” “EdgePointIncludedAngle”, ” - ” “LengthRatioOffset”, ” - ” “ParallelDeviation”, ” - ” “ShapeFactor”, ” - ” “Twist”, ” - ” “LengthMinimum”, ” - ” “LengthMaximum”, ” - ” “TetCollapse”, ” - ” “WarpageAngle”, ” - ” “CohesiveElement”, ” - ” “LaminateTaperRatio”, ” Ratio of longest edge to shortest edge instacking direction for the elements that reference PCOMPS entries only.”
“LaminateThicknessRatio”, ” Ratio of the difference between thicknessin stacking direction as defined by grids and thickness as defined by ply thickness specification to the thickness in the stacking direction as defined by grids for the elements that reference PCOMPS entries only.”
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-