SolidElementFaceNormalBuilder Class¶
-
class
NXOpen.CAE.ModelCheck.
SolidElementFaceNormalBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.ModelCheck.SolidElementFaceNormalBuilder
used to reorient normals for left handed solid elements.Both of the methods are only available in fem context.
To create a new instance of this class, use
NXOpen.CAE.ModelCheckManager.CreateSolidElementFaceNormalBuilder()
New in version NX11.0.0.
Properties¶
Property | Description |
---|---|
NegativeFaceColor | Returns or sets the negative face color |
PositiveFaceColor | Returns or sets the positive face color |
SelectionList | Returns the selected objects to be checked. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CreateGroupOfLeftHandedElements | Create group for the left handed elements in NXOpen.CAE.ModelCheck.SolidElementFaceNormalBuilder.CreateGroupOfLeftHandedElements() and returns those elements which were grouped successfully. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
DisplayNormals | Display normals of NXOpen.CAE.ModelCheck.SolidElementFaceNormalBuilder.DisplayNormals() |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ReorientLeftHandedElements | Reorient normals specified in NXOpen.CAE.ModelCheck.SolidElementFaceNormalBuilder.ReorientLeftHandedElements() which normal is left handed and returns those elements whose normals were reoriented successfully. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
NegativeFaceColor¶
-
SolidElementFaceNormalBuilder.
NegativeFaceColor
¶ Returns or sets the negative face color
-------------------------------------
Getter Method
Signature
NegativeFaceColor()
Returns: Return type: int New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
NegativeFaceColor(negativeFaceColor)
Parameters: negativeFaceColor (int) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
PositiveFaceColor¶
-
SolidElementFaceNormalBuilder.
PositiveFaceColor
¶ Returns or sets the positive face color
-------------------------------------
Getter Method
Signature
PositiveFaceColor()
Returns: Return type: int New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PositiveFaceColor(positiveFaceColor)
Parameters: positiveFaceColor (int) – New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SelectionList¶
-
SolidElementFaceNormalBuilder.
SelectionList
¶ Returns the selected objects to be checked.
The objects must be
NXOpen.CAE.Mesh
orNXOpen.CAE.FEElement
-------------------------------------
Getter Method
Signature
SelectionList()
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX11.0.0.
License requirements: None.
Method Detail¶
CreateGroupOfLeftHandedElements¶
-
SolidElementFaceNormalBuilder.
CreateGroupOfLeftHandedElements
¶ Create group for the left handed elements in
NXOpen.CAE.ModelCheck.SolidElementFaceNormalBuilder.CreateGroupOfLeftHandedElements()
and returns those elements which were grouped successfully.This method will only group left handed solid elements in the current work fem part.
Signature
CreateGroupOfLeftHandedElements()
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
DisplayNormals¶
-
SolidElementFaceNormalBuilder.
DisplayNormals
¶ Display normals of
NXOpen.CAE.ModelCheck.SolidElementFaceNormalBuilder.DisplayNormals()
Signature
DisplayNormals()
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ReorientLeftHandedElements¶
-
SolidElementFaceNormalBuilder.
ReorientLeftHandedElements
¶ Reorient normals specified in
NXOpen.CAE.ModelCheck.SolidElementFaceNormalBuilder.ReorientLeftHandedElements()
which normal is left handed and returns those elements whose normals were reoriented successfully.This method will only reorient the normals for solid left handed elements in the current work fem part.
Signature
ReorientLeftHandedElements()
New in version NX11.0.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Validate¶
-
SolidElementFaceNormalBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.