DuplicateElementsCheckBuilder Class¶
-
class
NXOpen.CAE.ModelCheck.
DuplicateElementsCheckBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.ModelCheck.DuplicateElementsCheckBuilder
to check for duplicate elements within the candidate elements.Duplicate elements are elements which share the same corner nodes,but do not include the middle nodes.
The general workflow is:
- Set the candidate elements
- Set the display settings data
- Identify the duplicate elements
- Set the preference option
- Delete the duplicate elements
You can delete duplicate elements through
Builder.Commit()
orNXOpen.CAE.ModelCheck.DuplicateElementsCheckBuilder.DeleteDuplicateElements()
. Commits the builder to delete duplicate elements.To create a new instance of this class, use
NXOpen.CAE.ModelCheckManager.CreateDuplicateElementsCheckBuilder()
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
DisplaySettingsData | Returns or sets the display settings for duplicate elements |
DuplicateElementGroupsCount | Returns the duplicate elements group count, each group contains elements that are duplicates of each other and each group contains at least two duplicate elements |
Preference | Returns or sets the duplicate elements deleting preference |
PreferenceElements | Returns the preference elements for keep selected and remove selected options |
SelectionList | Returns the selected objects to be checked. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
DeleteDuplicateElements | Deletes the duplicate elements and clear all cached duplicate elements in this builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDuplicateElements | Returns the duplicate elements of specified group index @return |
GetObject | Returns the object currently being edited by this builder. |
IdentifyDuplicateElements | Calculates to find the duplicate elements and display them in the NXOpen.CAE.ModelCheck.DuplicateElementsCheckBuilderDisplaySettings_Struct . |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
DuplicateElementsCheckBuilderDeletePreference Enumeration | Represents the duplicate elements deleting preference |
Structs¶
DuplicateElementsCheckBuilderDisplaySettings_Struct Struct | Represents the display settings of duplicated elements detected |
Property Detail¶
DisplaySettingsData¶
-
DuplicateElementsCheckBuilder.
DisplaySettingsData
¶ Returns or sets the display settings for duplicate elements
-------------------------------------
Getter Method
Signature
DisplaySettingsData()
Returns: Display settings data Return type: NXOpen.CAE.ModelCheck.DuplicateElementsCheckBuilderDisplaySettings_Struct
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DisplaySettingsData(displaySettings)
Parameters: displaySettings ( NXOpen.CAE.ModelCheck.DuplicateElementsCheckBuilderDisplaySettings_Struct
) – Display settings dataNew in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
DuplicateElementGroupsCount¶
-
DuplicateElementsCheckBuilder.
DuplicateElementGroupsCount
¶ Returns the duplicate elements group count, each group contains elements that are duplicates of each other and each group contains at least two duplicate elements
-------------------------------------
Getter Method
Signature
DuplicateElementGroupsCount()
Returns: Duplicate element groups count Return type: int New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Preference¶
-
DuplicateElementsCheckBuilder.
Preference
¶ Returns or sets the duplicate elements deleting preference
-------------------------------------
Getter Method
Signature
Preference()
Returns: Delete elements preference Return type: NXOpen.CAE.ModelCheck.DuplicateElementsCheckBuilderDeletePreference
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Preference(deletePreference)
Parameters: deletePreference ( NXOpen.CAE.ModelCheck.DuplicateElementsCheckBuilderDeletePreference
) – Delete elements preferenceNew in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
PreferenceElements¶
-
DuplicateElementsCheckBuilder.
PreferenceElements
¶ Returns the preference elements for keep selected and remove selected options
-------------------------------------
Getter Method
Signature
PreferenceElements()
Returns: Preference elements Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
SelectionList¶
-
DuplicateElementsCheckBuilder.
SelectionList
¶ Returns the selected objects to be checked.
The objects must be
NXOpen.CAE.Mesh
orNXOpen.CAE.FEElement
-------------------------------------
Getter Method
Signature
SelectionList()
Returns: Return type: NXOpen.SelectTaggedObjectList
New in version NX8.5.0.
License requirements: None.
Method Detail¶
DeleteDuplicateElements¶
-
DuplicateElementsCheckBuilder.
DeleteDuplicateElements
¶ Deletes the duplicate elements and clear all cached duplicate elements in this builder.
The method
Builder.Commit()
will also do the same thing. Duplicate elements can only be deleted when the context part of this builder is aNXOpen.CAE.BaseFemPart
Signature
DeleteDuplicateElements()
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”)
GetDuplicateElements¶
-
DuplicateElementsCheckBuilder.
GetDuplicateElements
¶ Returns the duplicate elements of specified group index
Signature
GetDuplicateElements(groupIndex)
Parameters: groupIndex (int) – Returns: Return type: list of NXOpen.CAE.FEElement
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
IdentifyDuplicateElements¶
-
DuplicateElementsCheckBuilder.
IdentifyDuplicateElements
¶ Calculates to find the duplicate elements and display them in the
NXOpen.CAE.ModelCheck.DuplicateElementsCheckBuilderDisplaySettings_Struct
.The detected duplicate elements are cached, to access the cached calculation result, you could use
NXOpen.CAE.ModelCheck.DuplicateElementsCheckBuilder.DuplicateElementGroupsCount`()
andNXOpen.CAE.ModelCheck.DuplicateElementsCheckBuilder.GetDuplicateElements()
. The previous cached data will be cleaned automatically when you start a new identification.Signature
IdentifyDuplicateElements()
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
Validate¶
-
DuplicateElementsCheckBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.