AlignShellElementNormalBuilder Class¶
-
class
NXOpen.CAE.ModelCheck.
AlignShellElementNormalBuilder
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAE.ModelCheck.AlignShellElementNormalBuilder
builder used to align the normals of connected shell elements with a seed shell element.You can align the normals by executing either
Builder.Commit()
orNXOpen.CAE.ModelCheck.AlignShellElementNormalBuilder.AlignNormals()
. The difference between these two methods isBuilder.Commit()
aligns the normals and updates normal display, but it does not return the elements that have changed normals.NXOpen.CAE.ModelCheck.AlignShellElementNormalBuilder.AlignNormals()
aligns the normals and returns the elements that have changed normals. Both of the methods are only available in fem context.To create a new instance of this class, use
NXOpen.CAE.ModelCheckManager.CreateAlignShellElementNormalBuilder()
New in version NX8.5.0.
Properties¶
Property | Description |
---|---|
ElementConnectScope | Returns or sets the option to indicate how to define connected elements for checking |
ReverseSeedNormal | Returns or sets the option indicating whether to reverse element normals so that they are aligned with the seed element |
SeedElement | Returns or sets the seed element |
Tag | Returns the Tag for this object. |
UserSpecifiedConnectElements | Returns the user specified connected elements to be aligned with seed element |
Methods¶
Method | Description |
---|---|
AlignNormals | Aligns the normals of elements connected to the seed element. |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
DisplayNormals | Display element normals for connected elements, which are to be aligned with seed element normal |
FindAllVisibleConnectedElements | Finds all visible elements connected with the seed element @return |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
AlignShellElementNormalBuilderConnectedElementScope Enumeration | the options to define the connection scope to the seed element for model checking |
Property Detail¶
ElementConnectScope¶
-
AlignShellElementNormalBuilder.
ElementConnectScope
¶ Returns or sets the option to indicate how to define connected elements for checking
-------------------------------------
Getter Method
Signature
ElementConnectScope()
Returns: Return type: NXOpen.CAE.ModelCheck.AlignShellElementNormalBuilderConnectedElementScope
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ElementConnectScope(connectScope)
Parameters: connectScope ( NXOpen.CAE.ModelCheck.AlignShellElementNormalBuilderConnectedElementScope
) –New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
ReverseSeedNormal¶
-
AlignShellElementNormalBuilder.
ReverseSeedNormal
¶ Returns or sets the option indicating whether to reverse element normals so that they are aligned with the seed element
-------------------------------------
Getter Method
Signature
ReverseSeedNormal()
Returns: Return type: bool New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReverseSeedNormal(seedNormalToBeReversed)
Parameters: seedNormalToBeReversed (bool) – New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
SeedElement¶
-
AlignShellElementNormalBuilder.
SeedElement
¶ Returns or sets the seed element
-------------------------------------
Getter Method
Signature
SeedElement()
Returns: Return type: NXOpen.CAE.FEElement
New in version NX8.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SeedElement(seedElement)
Parameters: seedElement ( NXOpen.CAE.FEElement
) –New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
UserSpecifiedConnectElements¶
-
AlignShellElementNormalBuilder.
UserSpecifiedConnectElements
¶ Returns the user specified connected elements to be aligned with seed element
-------------------------------------
Getter Method
Signature
UserSpecifiedConnectElements()
Returns: Return type: NXOpen.CAE.SelectElementsBuilder
New in version NX8.5.0.
License requirements: None.
Method Detail¶
AlignNormals¶
-
AlignShellElementNormalBuilder.
AlignNormals
¶ Aligns the normals of elements connected to the seed element.
Returns the elements that have had the normals successfully reversed. This method will only reverse the normals for shell elements in the current work fem part.
Signature
AlignNormals()
Returns: Return type: list of NXOpen.CAE.FEElement
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
DisplayNormals¶
-
AlignShellElementNormalBuilder.
DisplayNormals
¶ Display element normals for connected elements, which are to be aligned with seed element normal
Signature
DisplayNormals()
New in version NX8.5.0.
License requirements: nx_masterfem (“Finite Element Modeling”) OR nx_design_sim (“NX Design Simulation”)
FindAllVisibleConnectedElements¶
-
AlignShellElementNormalBuilder.
FindAllVisibleConnectedElements
¶ Finds all visible elements connected with the seed element
Signature
FindAllVisibleConnectedElements()
Returns: Return type: list of NXOpen.CAE.FEElement
New in version NX8.5.0.
License requirements: None.
Validate¶
-
AlignShellElementNormalBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.