TextComponent Class¶
-
class
NXOpen.Annotations.
TextComponent
¶ Bases:
NXOpen.TransientObject
Represents a single text in an annotation and can be queried for information about that text.
This information includes the type of text, the number of lines of text, the lines of text, and the origin in absolute coordinates. .. versionadded:: NX6.0.0
Properties¶
Property | Description |
---|---|
Height | Returns the text height. |
Length | Returns the text length. |
NumberLines | Returns the number of lines of text. |
Origin | Returns the text origin in absolute coordinates. |
Type | Returns the text type. |
Methods¶
Method | Description |
---|---|
Dispose | Free resources associated with the text component. |
GetDistanceToTop | The distance from the origin to the top of text. |
GetIntegerizedLength | The text integerized length. |
GetText | Gets all of the text for the text component. |
Enumerations¶
TextComponentTextType Enumeration | the text type. |
Property Detail¶
Height¶
-
TextComponent.
Height
¶ Returns the text height.
-------------------------------------
Getter Method
Signature
Height()
Returns: the text height Return type: float New in version NX6.0.0.
License requirements: None.
Length¶
-
TextComponent.
Length
¶ Returns the text length.
-------------------------------------
Getter Method
Signature
Length()
Returns: the text length Return type: float New in version NX6.0.0.
License requirements: None.
NumberLines¶
-
TextComponent.
NumberLines
¶ Returns the number of lines of text.
-------------------------------------
Getter Method
Signature
NumberLines()
Returns: the number of lines of text Return type: int New in version NX6.0.0.
License requirements: None.
Origin¶
-
TextComponent.
Origin
¶ Returns the text origin in absolute coordinates.
If the annotation is on a drawing, origin is returned in drawing space. If the annotation is on the model, origin is returned in model space.
-------------------------------------
Getter Method
Signature
Origin()
Returns: the text origin in absolute coordinates Return type: NXOpen.Point3d
New in version NX6.0.0.
License requirements: None.
Type¶
-
TextComponent.
Type
¶ Returns the text type.
-------------------------------------
Getter Method
Signature
Type()
Returns: the text type Return type: NXOpen.Annotations.TextComponentTextType
New in version NX6.0.0.
License requirements: None.
Method Detail¶
Dispose¶
-
TextComponent.
Dispose
¶ Free resources associated with the text component.
After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.
Signature
Dispose()
New in version NX6.0.0.
License requirements: None.
GetDistanceToTop¶
-
TextComponent.
GetDistanceToTop
¶ The distance from the origin to the top of text.
Signature
GetDistanceToTop()
Returns: the distance from the origin to the top of text Return type: float New in version NX6.0.0.
License requirements: None.