TextComponentTextType Enumeration¶
NXOpen.Annotations.TextComponent.TextType is an alias for NXOpen.Annotations.TextComponentTextType
-
class
NXOpen.Annotations.
TextComponentTextType
¶ Bases:
object
the text type.
Enum Members
Enum Member Enum Member Description Text primary dimension text or main text for draft aidsDualDimension dual dimension textTolerance tolerance textDualTolerance dual tolerance textDiameterRadius diameter or radius or arc length symbol textAppendedAbove appended text aboveAppendedBelow appended text belowAppendedBefore appended text beforeAppendedAfter appended text afterChamferBefore chamfer text beforeChamferAfter chamfer text afterChamferSize chamfer size textChamferXSymbol chamfer x symbol textChamferAngle chamfer angle symbol text-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-