TableStyleBuilder Class¶
-
class
NXOpen.Annotations.
TableStyleBuilder
¶ Bases:
NXOpen.Annotations.StyleBuilder
Represents a
NXOpen.Annotations.TableStyleBuilder
.This class is used to set Annotation preferences when creating or editing an annotation.
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
BendTable | Returns the Bend table settings builder |
BreakSettings | Returns the get break builder |
DimensionStyle | Returns the dimension style builder |
ForeshorteningSymbolSettings | Returns the get builder for foreshortening symbol |
FrameBarStyle | Returns the frame bar builder |
HatchStyle | Returns the hatch style builder |
HoleCalloutSettings | Returns the hole callout settings builder |
HoleTableContent | Returns the Hole table settings content builder |
HoleTableFormat | Returns the Hole table settings format builder |
HoleTableHoleFilters | Returns the Hole table settings hole filters builder |
HoleTableLabel | Returns the Hole table settings label builder |
HoleTableWorkflow | Returns the Hole table settings workflow builder |
LetteringStyle | Returns the lettering style builder |
LineArrowStyle | Returns the line/arrow style builder |
OrdinateStyle | Returns the ordinate style builder |
RadialStyle | Returns the radial style builder |
SingleSidedDisplay | Returns the single sided display builder |
SymbolStyle | Returns the symbol style builder |
TableCellStyle | Returns the cell style builder |
TableSectionStyle | Returns the section style builder |
TabularNoteStyle | Returns the tabular note style builder |
Tag | Returns the Tag for this object. |
UnitsStyle | Returns the units style builder |
Methods¶
Method | Description |
---|---|
InheritSettingsFromCustomerDefault | Inherit Settings From Customer Default |
InheritSettingsFromPreferences | Inherit Settings From Preference |
InheritSettingsFromSelectedObjects | Inherit Settings From Selected Objects |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BendTable¶
-
TableStyleBuilder.
BendTable
¶ Returns the Bend table settings builder
-------------------------------------
Getter Method
Signature
BendTable()
Returns: Return type: NXOpen.Annotations.BendTableSettingsBuilder
New in version NX9.0.0.
License requirements: None.
HoleTableContent¶
-
TableStyleBuilder.
HoleTableContent
¶ Returns the Hole table settings content builder
-------------------------------------
Getter Method
Signature
HoleTableContent()
Returns: Return type: NXOpen.Annotations.HoleTableSettingsContentBuilder
New in version NX9.0.0.
License requirements: None.
HoleTableFormat¶
-
TableStyleBuilder.
HoleTableFormat
¶ Returns the Hole table settings format builder
-------------------------------------
Getter Method
Signature
HoleTableFormat()
Returns: Return type: NXOpen.Annotations.HoleTableSettingsFormatBuilder
New in version NX9.0.0.
License requirements: None.
HoleTableHoleFilters¶
-
TableStyleBuilder.
HoleTableHoleFilters
¶ Returns the Hole table settings hole filters builder
-------------------------------------
Getter Method
Signature
HoleTableHoleFilters()
Returns: Return type: NXOpen.Annotations.HoleTableSettingsHoleFiltersBuilder
New in version NX9.0.0.
License requirements: None.
HoleTableLabel¶
-
TableStyleBuilder.
HoleTableLabel
¶ Returns the Hole table settings label builder
-------------------------------------
Getter Method
Signature
HoleTableLabel()
Returns: Return type: NXOpen.Annotations.HoleTableSettingsLabelBuilder
New in version NX9.0.0.
License requirements: None.
HoleTableWorkflow¶
-
TableStyleBuilder.
HoleTableWorkflow
¶ Returns the Hole table settings workflow builder
-------------------------------------
Getter Method
Signature
HoleTableWorkflow()
Returns: Return type: NXOpen.Annotations.HoleTableSettingsWorkflowBuilder
New in version NX9.0.0.
License requirements: None.
TableCellStyle¶
-
TableStyleBuilder.
TableCellStyle
¶ Returns the cell style builder
-------------------------------------
Getter Method
Signature
TableCellStyle()
Returns: Return type: NXOpen.Annotations.TableCellStyleBuilder
New in version NX6.0.0.
License requirements: None.
TableSectionStyle¶
-
TableStyleBuilder.
TableSectionStyle
¶ Returns the section style builder
-------------------------------------
Getter Method
Signature
TableSectionStyle()
Returns: Return type: NXOpen.Annotations.TableSectionStyleBuilder
New in version NX8.0.0.
License requirements: None.
TabularNoteStyle¶
-
TableStyleBuilder.
TabularNoteStyle
¶ Returns the tabular note style builder
-------------------------------------
Getter Method
Signature
TabularNoteStyle()
Returns: Return type: NXOpen.Annotations.TabularNoteStyleBuilder
New in version NX8.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
TableStyleBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.