TabularNoteStyleBuilder Class

class NXOpen.Annotations.TabularNoteStyleBuilder

Bases: NXOpen.TaggedObject, NXOpen.GeometricUtilities.IComponentBuilder

Represents a NXOpen.Annotations.TabularNoteStyleBuilder.

New in version NX8.0.0.

Properties

Property Description
AutomaticUpdate Returns or sets the automatic update
LockTableContents Returns or sets the lock table contents
LockTableFormat Returns or sets the lock table format
ShowLockedDeletedContent Returns or sets the locked deleted row method
Tag Returns the Tag for this object.

Methods

Method Description
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Enumerations

TabularNoteStyleBuilderShowLockedDeletedRowMethod Enumeration the valid locked deleted row methods

Property Detail

AutomaticUpdate

TabularNoteStyleBuilder.AutomaticUpdate

Returns or sets the automatic update

-------------------------------------

Getter Method

Signature AutomaticUpdate()

Returns:
Return type:bool

New in version NX8.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature AutomaticUpdate(automaticUpdate)

Parameters:automaticUpdate (bool) –

New in version NX8.0.0.

License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)

LockTableContents

TabularNoteStyleBuilder.LockTableContents

Returns or sets the lock table contents

-------------------------------------

Getter Method

Signature LockTableContents()

Returns:
Return type:bool

New in version NX8.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature LockTableContents(lockedTableContents)

Parameters:lockedTableContents (bool) –

New in version NX8.0.0.

License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)

LockTableFormat

TabularNoteStyleBuilder.LockTableFormat

Returns or sets the lock table format

-------------------------------------

Getter Method

Signature LockTableFormat()

Returns:
Return type:bool

New in version NX8.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature LockTableFormat(lockedTableFormat)

Parameters:lockedTableFormat (bool) –

New in version NX8.0.0.

License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)

ShowLockedDeletedContent

TabularNoteStyleBuilder.ShowLockedDeletedContent

Returns or sets the locked deleted row method

-------------------------------------

Getter Method

Signature ShowLockedDeletedContent()

Returns:
Return type:NXOpen.Annotations.TabularNoteStyleBuilderShowLockedDeletedRowMethod

New in version NX8.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature ShowLockedDeletedContent(showLockedDeletedContent)

Parameters:showLockedDeletedContent (NXOpen.Annotations.TabularNoteStyleBuilderShowLockedDeletedRowMethod) –

New in version NX8.0.0.

License requirements: geometric_tol (“GDT”) OR drafting (“DRAFTING”)

Method Detail

Validate

TabularNoteStyleBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.